need Mictor connector test board for IMX6SL EVK board

cancel
Showing results for 
Search instead for 
Did you mean: 

need Mictor connector test board for IMX6SL EVK board

108 Views
danmez
Contributor I

I need to develop a small test circuit and connect to some GPIO on the IMX6SL EVK development board.  The signals I need to use are on the Mictor connector on the EVK.

Can someone recommend a small test board that is available off the shelf?  Ideally it would have the mating Mictor connector on one side and bring the signals to some larger connector or header so I can make easy connections.  If it had a little proto board that would be nice as well.

Thanks!

Labels (1)
0 Kudos
0 Replies