my imx8mplus custom board unable to read the video

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

my imx8mplus custom board unable to read the video

223 Views
srinivas_123
Contributor III

I am using an i.MX8M Plus custom board. I have a requirement to read a video that is already present in my rootfs folder and create frames from that video.

i am using 0v5640 camera  on both boards(custom and evk).

I built the imx-image-full image, which includes all libraries and packages.

On the i.MX8M Plus LPDDR4 EVK, my application runs properly and creates the frames.

On the i.MX8M Plus custom board, I encounter the following error messages:


[ 335.510360] e00000001 got error -2
[ WARN:0@8.573] global cap_gstreamer.cpp:2784 handleMessage OpenCV | GStreamer warning: Embedded video playback halted; module v4l2h264dec0 reported: Could not read from resource.
[ WARN:0@8.578] global cap_gstreamer.cpp:1679 open OpenCV | GStreamer warning: unable to start pipeline
[ WARN:0@8.578] global cap_gstreamer.cpp:1164 isPipelinePlaying OpenCV | GStreamer warning: GStreamer: pipeline has not been created
[ WARN:0@8.812] global cap_gstreamer.cpp:2563 open OpenCV | GStreamer warning: cannot link elements

Why is this happening? Could anyone please help me out?

If anyone has suggestions on approaches to resolve this issue, please let me know. I have also attached the application.


Thanks&Regards

Srinivas

0 Kudos
Reply
1 Reply

204 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Since it works on EVK, I guess this can be due to a bad image building per the error it looks like you don't have openCV, or you are not able to read the camera.

Regards

0 Kudos
Reply