mxc_i2c_slave_test fails

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mxc_i2c_slave_test fails

2,970件の閲覧回数
djoygaurav
Contributor II

Hi,

 

I am trying to test i.mx6 i2c test(mxc_i2c_slave_test) on i.mx6 Ultra Lite EVK board but can't figure out the test code flow and any specific steps I need to follow(if required). The test is failing upon execution of "mxc_i2c_slave_test.out" file and the log I am getting is:

 

root@imx6ulevk:/unit_tests# ./mxc_i2c_slave_test.out

i2c-slave-test:open device error

i2c-slave-test: slave thread: Fail

i2c-slave-test:master thread:about to receive 100 bytes

i2c-slave-test:master thread: read error

i2c-slave-test:master thread: Fail

 

Also, in the source code "mxc_i2c_slave_test.c", there is I2C Slave(macro "I2C_SLAVE_DEV") which is mapping to "/dev/slave-i2c-0" but there's no such node present in my "/dev/". Can someone please help me on this?

ラベル(3)
タグ(2)
2 返答(返信)

2,418件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Gaurav

please check Chapter 35 Inter-IC (I2C) Driver attached Linux Manual,

also may be useful link

https://community.nxp.com/message/599314

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,418件の閲覧回数
djoygaurav
Contributor II

Thank You Igor.

0 件の賞賛
返信