mx7d with ar8035 can not work go on

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx7d with ar8035 can not work go on

1,203 Views
xing
Contributor I

Can not attachment file when community reply ?

mx7d with ar8035 can not work  

Original Attachment has been moved to: wiseiot.c.zip

Original Attachment has been moved to: imx7d-wiseiot.dts.zip

Labels (1)
0 Kudos
Reply
2 Replies

1,049 Views
xing
Contributor I

HI Wigros Sun,

Thank you reply.

I have update mach-imx7d file. 

and wiseiot.c is my custom uboot file.

please refer to the issure:

imx7d with ar8035 can not work 

0 Kudos
Reply

1,049 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Tianxin,

    I checked your dts file, which is no problem. But I don't understand  wiseiot.c file you pasted, because most of porting job should be done in device tree!

    for AR8035 and fec init, they should be in mach-imx7d.c file, the file is the entry of the board. you should add ar8035 init source code into the file.

    you can refer to the mach-imx6q.c, and copy ar8035 source code to mach-imx7d. then debug it.

  

    Hope above advice can help you!


Have a great day,
TIC    Weidong Sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply