mx6q can support dual usb uvc camera in android 4.3 system?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mx6q can support dual usb uvc camera in android 4.3 system?

ソリューションへジャンプ
1,231件の閲覧回数
mrleo
Contributor IV

Hi all,

    My custom board is mx6q board,I want support two usb uvc camera.

    One is ok for me,please help me how to support two usb uvc camera?

    Can it open at the same time?

Thanks,

Leo

ラベル(7)
0 件の賞賛
1 解決策
773件の閲覧回数
mrleo
Contributor IV

Hi Victor Linnik,

So two usb camera can't support in android.But can support in linux system.

Thanks Very much!

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
774件の閲覧回数
mrleo
Contributor IV

Hi Victor Linnik,

So two usb camera can't support in android.But can support in linux system.

Thanks Very much!

0 件の賞賛
773件の閲覧回数
b36401
NXP Employee
NXP Employee

You can connect 2 USB cameras to i.MX6 fine.

Please refer "Using a USB Camera with GStreamer" document

https://community.freescale.com/docs/DOC-93688

regarding connecting the cameras.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛