mx6dl ddr_test write level issu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx6dl ddr_test write level issu

2,258 Views
chuanyanyin
Contributor III

Hi All:

 

  I use my custom board to run ddr stress test v1.0.3,  The DDR3 is H5TQ2G63BFR,  tRCD=tRP=CL (ns) =  15, tRC = 52.5, tRAS = 37.5, When the CPU is MX6Q, everything is fine. When I test other board which  the CPU is MCIMX6U5DVM10AB, the WL is larger than 0x2F:

Would you like to run the write leveling calibration? (y/n)

  Please enter the MR1 value on the initilization script

  This will be re-programmed into MR1 after write leveling calibration

  Enter as a 4-digit HEX value, example 0004, then hit enter

0004 You have entered: 0x0004

Start write leveling calibration

Write leveling calibration completed

MMDC_MPWLDECTRL0 ch0 after write level cal: 0x004A004D

MMDC_MPWLDECTRL1 ch0 after write level cal: 0x003F0043

MMDC_MPWLDECTRL0 ch1 after write level cal: 0x001F0025

MMDC_MPWLDECTRL1 ch1 after write level cal: 0x0022003B

I'm sure  WALAT bit  of MMDCx_MDMISC is 1(0x021b0018 = 0x00011740) ,  The i.MX6_DDR_Stress_Test_User_Guide.pdf said

"If write-leveling delay is larger than 0x2f, it is suggested to

set the WALAT value on MMDCx_MDMISC register to 1 in

the initialization script and re-run the DDR_Stress_Tester".

Hower, the stress test can passed.

WL is larger than 0x2F , I Can't  make WL smaller than 0x2F. Can it cause any problem with MX6DL?

Original Attachment has been moved to: ddr_stress_test_for_dl.txt.zip

Original Attachment has been moved to: test.inc.txt.zip

Labels (3)
0 Kudos
Reply
3 Replies

1,941 Views
igorpadykov
NXP Employee
NXP Employee

Hi chuanyan

yes can leave WALAT=0 after thorough board testing, however

it is recommended to set it to 1, since in rare cases, seems it may violate

DDR datasheets waveforms as explained below.

https://community.freescale.com/message/381090#381090

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,941 Views
chuanyanyin
Contributor III

Hi igor:

   I have let WALAT=0 already, but  the result is almost same.

0004 You have entered: 0x0004

Start write leveling calibration

Write leveling calibration completed

MMDC_MPWLDECTRL0 ch0 after write level cal: 0x003F0045

MMDC_MPWLDECTRL1 ch0 after write level cal: 0x0034003F

MMDC_MPWLDECTRL0 ch1 after write level cal: 0x00180016

MMDC_MPWLDECTRL1 ch1 after write level cal: 0x0013002A

When I put this value(I'm not sure it is correct ) into the flashheader.S, the Android System is not stable, it sometimes hung with  no logs displayed.

Has anyone run ddr test on DL board? I have heard that MX6DL is not stable as MX6Q, is it true?

0 Kudos
Reply

1,941 Views
igorpadykov
NXP Employee
NXP Employee

Hi chuanyan

instability may be used also by other factors, including bad power

supplies and wrong software configuration.

BTW had you applied latest GPU patches ? They are very critical for

stability:  IMX6LXPATCHRN

Please try software from DL dedicated page, for example

Demo

L3.0.35_4.1.0_DEMO_IMAGE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux Binary Demo Files.

i.MX6DL|i.MX 6DualLite Processors|3D Graphics|Freescale

then try to build min. Linux image and check it

L3.0.35_4.1.0_ER_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.

~igor

0 Kudos
Reply