Hi all,
I come across a problem. I initialize the AUART2.RTS pin(Bank 3, ID 11), and enable it to be a output GPIO pin. At the same time, enable the pull up function. But when I read out the HW_PINCTRL_PULL3 register. I get all 0. The settings in others register like MUX, DOUT, DRIVE and DOE are quite normal. I haven't modified the pinctrl.c file. It's original.
Why this happens?
{
.name = "AUART2.RTS",
.id = PINID_AUART2_RTS,
.fun = PIN_GPIO,
.strength = PAD_4MA,
.voltage = PAD_3_3V,
.drive = 1,
.pullup = 1,
.pull = 1,
.output = 1,
.data = 0,
},
One more question, does the pull up function affect the GPIO's output? According to the MX28RM, it only disable the gate keeper.
Thanks in advance.
解決済! 解決策の投稿を見る。
Hi h k
pull up function does not affect the GPIO's output, however
not all pads have pul-ups, only described in
Table 9-3. i.MX28 Functions with Pullup Resistors MX28RM
http://cache.freescale.com/files/dsp/doc/ref_manual/MCIMX28RM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi h k
pull up function does not affect the GPIO's output, however
not all pads have pul-ups, only described in
Table 9-3. i.MX28 Functions with Pullup Resistors MX28RM
http://cache.freescale.com/files/dsp/doc/ref_manual/MCIMX28RM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------