Hi all,
I have a mx28evk board with a Micron MT29F1G08ABADAWP Nand flash. Totally 128MB and 2K + 64 page size. When I update the firmware using MFGTool, I keep seeing the "Attempt to write not page aligned data" error.
NFC: Version 1, 8-chip GPMI and BCH
Boot ROM: Version 1, Single-chip boot area, block mark swapping supported
Scanning for NAND Flash chips...
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xf1 (Micron NAND 128MiB 3,3V 8-bit)
-----------------------------
NAND Flash Device Information
-----------------------------
Manufacturer : Micron (0x2c)
Device Code : 0xf1
Cell Technology : SLC
Chip Size : 128 MiB
Pages per Block : 64
Page Geometry : 2048+64
ECC Strength : 4 bits
ECC Size : 512 B
Data Setup Time : 10 ns
Data Hold Time : 7 ns
Address Setup Time: 15 ns
GPMI Sample Delay : 6 ns
tREA : Unknown
tRLOH : Unknown
tRHOH : Unknown
Description : MT29F1G08ABADAWP
-----------------
Physical Geometry
-----------------
Chip Count : 1
Page Data Size in Bytes: 2048 (0x800)
Page OOB Size in Bytes : 64
Block Size in Bytes : 131072 (0x20000)
Block Size in Pages : 64 (0x40)
Chip Size in Bytes : 134217728 (0x8000000)
Chip Size in Pages : 65536 (0x10000)
Chip Size in Blocks : 1024 (0x400)
Medium Size in Bytes : 134217728 (0x8000000)
------------
NFC Geometry
------------
ECC Algorithm : BCH
ECC Strength : 8
Page Size in Bytes : 2112
Metadata Size in Bytes : 10
ECC Chunk Size in Bytes: 512
ECC Chunk Count : 4
Payload Size in Bytes : 2048
Auxiliary Size in Bytes: 16
Auxiliary Status Offset: 12
Block Mark Byte Offset : 1999
Block Mark Bit Offset : 0
-----------------
Boot ROM Geometry
-----------------
Boot Area Count : 1
Boot Area Size in Bytes : 20971520 (0x1400000)
Stride Size in Pages : 64
Search Area Stride Exponent: 2
Scanning device for bad blocks
Boot area protection is enabled.
Creating 2 MTD partitions on "gpmi-nfc-main":
0x000000000000-0x000001400000 : "gpmi-nfc-0-boot"
0x000001400000-0x000008000000 : "gpmi-nfc-general-use"
regulator_init_complete: incomplete constraints, leaving vbus5v on
mxs-rtc mxs-rtc.0: setting system clock to 1970-01-01 00:00:48 UTC (48)
Freeing init memory: 176K
Starting UTP
disable turn off display
uuc 0.4 [built Feb 21 2014 08:19:00]
UTP: Waiting for device to appear
utp_mk_devnode: creating node '/dev/utp' with 10+222
cpu_id is 28
g_file_storage gadget: high speed config #1
UTP: received command 'mknod class/mtd,mtd0,/dev/mtd0'
class = 'class/mtd'
item = 'mtd0'
node = /dev/mtd0
type = (null)
UTP: running utp_mk_devnode(class/mtd,mtd0,/dev/mtd0,0x2000)
utp_mk_devnode: creating node '/dev/mtd0' with 90+0
UTP: sending Success
UTP: received command 'mknod class/mtd,mtd1,/dev/mtd1'
class = 'class/mtd'
item = 'mtd1'
node = /dev/mtd1
type = (null)
UTP: running utp_mk_devnode(class/mtd,mtd1,/dev/mtd1,0x2000)
utp_mk_devnode: creating node '/dev/mtd1' with 90+2
UTP: sending Success
UTP: received command 'mknod class/misc,ubi_ctrl,/dev/ubi_ctrl'
class = 'class/misc'
item = 'ubi_ctrl'
node = /dev/ubi_ctrl
type = (null)
UTP: running utp_mk_devnode(class/misc,ubi_ctrl,/dev/ubi_ctrl,0x2000)
utp_mk_devnode: creating node '/dev/ubi_ctrl' with 10+60
UTP: sending Success
UTP: received command '$ flash_eraseall /dev/mtd0'
UTP: sending Busy
UTP: executing "flash_eraseall /dev/mtd0"
Erautp_poll: pass returned. -- 68 % complete.
Erasing 128 Kibyte @ 1400000 -- 100 % complete.
UTP: sending Success
UTP: received command '$ flash_eraseall /dev/mtd1'
UTP: sending Busy
UTP: executing "flash_eraseall /dev/mtd1"
Erasing 128 Kibyte @ 6c00000 -- 100 % complete.
UTP: sending Success
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success
UTP: received command '$ dd if=$FILE of=/dev/mtd0'
UTP: sending Busy
UTP: executing "dd if=$FILE of=/dev/mtd0"
nand_do_write_ops: Attempt to write not page aligned data
dd: writing '/dev/mtd0': Invalid argument
1+0 records in
0+0 records out
UTP: sending Non-success
utp_poll: exit with status 256
Someone knows what happened? Kernel version is 2.6.35.3
I just add the flash's nand_device_info entry in nand_device_info.c. Except this nothing changed with nand driver.
Thanks in advance!
{
.end_of_table = false,
.manufacturer_code = 0x2c,
.device_code = 0xf1,
.cell_technology = NAND_DEVICE_CELL_TECH_SLC,
.chip_size_in_bytes = 128LL*SZ_1M,
.block_size_in_pages = 64,
.page_total_size_in_bytes = 2*SZ_1K + 64,
.ecc_strength_in_bits = 4,
.ecc_size_in_bytes = 512,
.data_setup_in_ns = 10,
.data_hold_in_ns = 7,
.address_setup_in_ns = 15,
.gpmi_sample_delay_in_ns = 6,
.tREA_in_ns = -1,
.tRLOH_in_ns = -1,
.tRHOH_in_ns = -1,
"MT29F1G08ABADAWP",
},
已解决! 转到解答。
I try to use another command: $ kobs-ng init $FILE in ucl.xml, this time the aligned error disappear, but with a new one problem: Couldn't discover Boot ROM version
Still don't know what has happened.