multiple displays on imx6 solo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

multiple displays on imx6 solo

ソリューションへジャンプ
1,089件の閲覧回数
jaiganesh
Contributor III

Hello there,

                    I would like to know what is the maximum number of displays that can be connected to imx6 solo processor.

                    As far as I know, in imx6 quad, we can connect upto 4 displays and I guess this is because of 2 IPUs available in the quad processor. Since we have only one IPU in imx6 solo processor, I would like to confirm on this.

Thanks,

Jai Ganesh S

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 解決策
801件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jai

I think 3 displays: IPU (2 Display Interfaces, may be routed to MIPI,LDB or HDMI) and EPDC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
802件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jai

I think 3 displays: IPU (2 Display Interfaces, may be routed to MIPI,LDB or HDMI) and EPDC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信