mplayer and ALSA audio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mplayer and ALSA audio

6,640 Views
iMxGuy
Contributor II

Hi,

mplayer is not outputing audio to my sound device. I am able to play sounds using aplay and mp3play, but with mplayer I get no sound. mplayer -ao shows the following output. I don't see ALSA listed. How can I get ALSA support for mplayer?

 

root@freescale ~$ mplayer -ao help
MPlayer 1.0rc2-4.4.4 (C) 2000-2007 MPlayer Team
Available audio output drivers:
oss OSS/ioctl audio output
mpegpes DVB audio output
v4l2 V4L2 MPEG Audio Decoder output
null Null audio output
pcm RAW PCM/WAVE file writer audio output

Labels (1)
0 Kudos
Reply
5 Replies

4,278 Views
小辉尤
Contributor III

hi:

     I have the same quesition!  why?

mplay

Mplay can play  all video format well,but the voice is not normal!!

(test:  mp4--OK ts--ok    wmv--ok  flv--ok  wma--ok avi--ok mkv--ok  rmvb--ok ,swf--no)

root@freescale ~$ mplayer -ao help

MPlayer 1.0rc2-4.4.4 (C) 2000-2007 MPlayer Team

Available audio output drivers:

oss OSS/ioctl audio output

mpegpes DVB audio output

v4l2 V4L2 MPEG Audio Decoder output

null Null audio output

pcm RAW PCM/WAVE file writer audio output

0 Kudos
Reply

4,277 Views
FS1z
Contributor II

Hi,

 

I assumed this ;-) I added the mplayer package in ltib and built it for the target imx28evk. Below you can find the configure output during ltib build of the mplayer package. As you can see, the ALSA lib was not found. So I guess that the development libraries/sources e.g. libasound2-dev and the header file alsa/asoundlib.h are missing.

 

Cheers,

F

 

cd mplayer-1.0~rc2

+ ./configure --cc=m68k-uclinux-gcc '--host-cc=ccache /usr/bin/gcc -B/usr/bin/' --enable-cross-compile --target=m68k-uclinux --disable-dvdread --enable-fbdev --disable-mencoder --enable-libavcodec_a --enable-libavutil_a --enable-libavformat_a --enable-libpostproc_a --enable-liba52 --disable-mp3lib --enable-static --disable-gui --disable-ivtv --disable-live --disable-dvdnav --disable-dvdread --disable-dvdread-internal --disable-libdvdcss-internal
Detected operating system: uclinux
Detected host architecture: m68k
Checking for m68k-uclinux-gcc version ... not found
Checking for gcc version ... 4.4.4, ok
Checking for host cc ... ccache /usr/bin/gcc -B/usr/bin/
Checking for cross compilation ... yes
Checking for assembler support of -pipe option ... yes
Checking for compiler support of named assembler arguments ... yes
Checking for .align is a power of two ... yes
Checking for -lposix ... no
Checking for -lm ... yes
Checking for langinfo ... yes
Checking for language ... using en (man pages: en )
Checking for enable sighandler ... yes
Checking for runtime cpudetection ... no
Checking for restrict keyword ... __restrict
Checking for __builtin_expect ... yes
Checking for kstat ... no
Checking for posix4 ... no
Checking for lrintf ... yes
Checking for mkstemp ... yes
Checking for nanosleep ... yes
Checking for socklib ... yes
Checking for inet_pton() ... yes (using )
Checking for network ... yes
Checking for inttypes.h (required) ... yes
Checking for int_fastXY_t in inttypes.h ... yes
Checking for word size ... ./configure: line 2967: /tmp/mplayer-conf-9294-8118: cannot execute binary file

Checking for malloc.h ... yes
Checking for memalign() ... yes
Checking for alloca.h ... yes
Checking for mman.h ... yes
Checking for dynamic loader ... yes
Checking for dynamic a/v plugins support ... no
Checking for pthread ... yes (using -lpthread)
Checking for w32threads ... no (using pthread instead)
Checking for rpath ... no
Checking for iconv ... yes
Checking for soundcard.h ... yes (sys/soundcard.h)
Checking for sys/dvdio.h ... no
Checking for sys/cdio.h ... no
Checking for linux/cdrom.h ... yes
Checking for dvd.h ... no
Checking for termcap ... no
Checking for termios ... no
Checking for shm ... yes
Checking for strsep() ... yes
Checking for vsscanf() ... yes
Checking for swab() ... yes
Checking for POSIX select() ... yes
Checking for gettimeofday() ... yes
Checking for glob() ... yes
Checking for setenv() ... yes
Checking for sys/sysinfo.h ... yes
Checking for pkg-config ... yes
Checking for Samba support (libsmbclient) ... no
Checking for tdfxfb ... no
Checking for s3fb ... no
Checking for tdfxvid ... no
Checking for xvr100 ... no
Checking for tga ... yes
Checking for md5sum support ... yes
Checking for bl ... no
Checking for DirectFB ... no
Checking for X11 headers presence ... yes
Checking for X11 ... no (check if the dev(el) packages are installed)
Checking for DPMS ... no
Checking for Xv ... no
Checking for XvMC ... no
Checking for Xinerama ... no
Checking for Xxf86vm ... no
Checking for XF86keysym ... no
Checking for DGA ... no
Checking for 3dfx ... no
Checking for OpenGL ... no
Checking for VIDIX ... no
Checking for /dev/mga_vid ... no
Checking for xmga ... no
Checking for GGI ... no
Checking for GGI extension: libggiwmh ... no
Checking for AA ... no
Checking for CACA ... no
Checking for SVGAlib ... no
Checking for FBDev ... yes
Checking for DVB ... no
Checking for DVB HEAD ... yes
Checking for zr ... no
Checking for PNG support ... no
Checking for JPEG support ... no
Checking for PNM support ... yes
Checking for GIF support ... no
Checking for VESA support ... no
Checking for SDL ... no
Checking for NAS ... no
Checking for DXR2 ... no
Checking for DXR3/H+ ... no
Checking for IVTV TV-Out ... no
Checking for V4L2 MPEG Decoder ... yes
Checking for OSS Audio ... yes
Checking for aRts ... no
Checking for EsounD ... Package esound was not found in the pkg-config search path.
Perhaps you should add the directory containing `esound.pc'
to the PKG_CONFIG_PATH environment variable
No package 'esound' found
Package esound was not found in the pkg-config search path.
Perhaps you should add the directory containing `esound.pc'
to the PKG_CONFIG_PATH environment variable
No package 'esound' found
no
Checking for Polyp ... no
Checking for JACK ... no
Checking for OpenAL ... no
Checking for ALSA audio ... no
Checking for Sun audio ... no
Checking for VCD support ... yes
Checking for dvdread ... no
Checking for internal libdvdcss ... no
Checking for cdparanoia ... no
Checking for libcdio ... no
Checking for bitmap font support ... yes
Checking for freetype >= 2.0.9 ... no
Checking for fontconfig ... no (freetype support needed)
Checking for SSA/ASS support ... no (FreeType support needed)
Checking for fribidi with charsets ... no
Checking for ENCA ... no
Checking for zlib ... yes
Checking for RTC ... yes
Checking for liblzo2 support ... yes
Checking for mad support ... no
Checking for Twolame ... no
Checking for Toolame ... no
Checking for OggVorbis support ... yes (internal Tremor)
Checking for libspeex (version >= 1.1 required) ... no
Checking for OggTheora support ... no
Checking for internal mp3lib support ... yes
Checking for internal liba52 support ... yes
Checking for libdca support ... no
Checking for internal libmpeg2 support ... yes
Checking for libmpcdec (musepack, version >= 1.2.1 required) ... no
Checking for FAAC (AAC encoder) support ... no (in libavcodec: )
Checking for FAAD2 (AAC) support ... yes (internal floating-point)
Checking for LADSPA plugin support ... no
Checking for Win32 codecs ... no
Checking for XAnim codecs ... yes (using /usr/local/lib/codecs)
Checking for RealPlayer codecs ... yes (using /usr/local/lib/codecs)
Checking for QuickTime codecs ... auto
Checking for Nemesi Streaming Media libraries ... no
Checking for LIVE555 Streaming Media libraries ... no
Checking for FFmpeg libavutil ... yes
Checking for FFmpeg libavcodec ... yes (libavcodec.so is discouraged over static libavcodec)
Checking for FFmpeg libavformat ... yes
Checking for FFmpeg libpostproc ... yes
Checking for libamr narrowband ... no
Checking for libamr wideband ... no
Checking for libdv-0.9.5+ ... no
Checking for XviD ... no
Checking for x264 ... no (in libavcodec: no)
Checking for libnut ... no
Checking for mencoder ... no
Checking for fastmemcpy ... yes
Checking for UniquE RAR File Library ... yes
Checking for TV interface ... yes
Checking for Video 4 Linux TV interface ... yes
Checking for Video 4 Linux 2 TV interface ... yes
Checking for TV teletext interface ... no
Checking for Radio interface ... no
Checking for Capture for Radio interface ... no
Checking for Video 4 Linux 2 Radio interface ... no
Checking for Video 4 Linux Radio interface ... no
Checking for Video 4 Linux 2 MPEG PVR interface ... yes
Checking for audio select() ... yes
Checking for ftp ... yes
Checking for vstream client ... no
Checking for byte order ... little-endian
Checking for OSD menu ... no
Checking for Subtitles sorting ... yes
Checking for XMMS inputplugin support ... no
Checking for inet6 ... yes
Checking for gethostbyname2 ... yes
Checking for GUI ... no
Checking for automatic gdb attach ... no
Checking for compiler support for noexecstack ... yes
Checking for joystick ... no
Checking for lirc ... no
Checking for lircc ... no
Checking for color console output ... no
Checking for DVD support (libdvdnav) ... no
Creating config.mak
Creating config.h

Config files successfully generated by ./configure --cc=m68k-uclinux-gcc --host-cc=ccache /usr/bin/gcc -B/usr/bin/ --enable-cross-compile --target=m68k-uclinux --disable-dvdread --enable-fbdev --disable-mencoder --enable-libavcodec_a --enable-libavutil_a --enable-libavformat_a --enable-libpostproc_a --enable-liba52 --disable-mp3lib --enable-static --disable-gui --disable-ivtv --disable-live --disable-dvdnav --disable-dvdread --disable-dvdread-internal --disable-libdvdcss-internal !

0 Kudos
Reply

4,278 Views
小辉尤
Contributor III

hi:

I am in accordance with your method tried, but the question remains!


IMX 535:

mplay

Mplay can play  all video format well,but the voice is not normal!!

(test:  mp4--OK ts--ok    wmv--ok  flv--ok  wma--ok avi--ok mkv--ok  rmvb--ok ,swf--no)

root@freescale ~$ mplayer -ao help

MPlayer 1.0rc2-4.4.4 (C) 2000-2007 MPlayer Team

Available audio output drivers:

oss OSS/ioctl audio output

mpegpes DVB audio output

v4l2 V4L2 MPEG Audio Decoder output

null Null audio output

pcm RAW PCM/WAVE file writer audio output

0 Kudos
Reply

4,278 Views
iMxGuy
Contributor II
I should have said, I was running mplayer on our i.MX28 board, not on my host machine.
0 Kudos
Reply

4,278 Views
FS1z
Contributor II

Hi,

the following helped for me, though I worked on a ubuntu platform

For Mplayer Alsa-support you'll need the libasound2-dev 
If you run the mplayer ./configure script it will report 
Checking for ALSA audio ... yes (using alsa 1.0.x and alsa/asoundlib.h)
Greetings,
F
0 Kudos
Reply