moving console to microusb on imx6ull EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

moving console to microusb on imx6ull EVK

997件の閲覧回数
asurti9
Contributor III

Hello community,

Is there a possibility of moving console (UART) to microusb port? Such that there is dual functionality on USB port?

Thanks!

タグ(3)
0 件の賞賛
返信
2 返答(返信)

948件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

i.MX 6ULL Applications Processors contains two high speed (HS) USB 2.0 OTG (Up to 480 Mbps) controllers, with two integrated HS USB Phy. On the EVK board, J1101 is a Type-A connector for USB host port, J1102 is a Micro-B connector for USB OTG port. The OTG port J1102 is also used for downloading the boot image by UUU Tool in Serial Download Mode.

0 件の賞賛
返信

950件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

No, for the i.MX6ULL recommend to use the UART to debug, you can see that in our EVK we use the UART TO USB to debug easily.

0 件の賞賛
返信