imx6q 4.1.15 kenel
when I modprobe fec , caused smsc95xx 'USB disconnect' and unregistered then register ,
I want to know the reason.
解決済! 解決策の投稿を見る。
I found the reason that problem actually was caused by hardware. I need to change device tree of 'regulator' part ,
I found the reason that problem actually was caused by hardware. I need to change device tree of 'regulator' part ,
actually I want change eth0 to eth1 & eth0 to eth1, normally fec initialize at first, I compile fec && smsc95xx as module to change the sequence . it is ok in imx8 4.19,but in imx6q 4.1.15 when I modprobe fec, causing smsc95xx reset , I couldn't change the eth0 eth1 sequence
thanks for your docment. I'll try KGDB . I have tried ftrace tools . It bothers me a lot ,because on our imx8mm board 4.19 kernel , it didn't happen , I can modprobe fec and won't influence the smsc95xx.
in general one can check if smsc95xx driver is built into the kernel ("=y") or built
as a module ("=m") or is not selected.
Best regards
igor
On imx8 4.19 I have no trouble.
Hi Bill
one can try to rebuild all image from scratch, reset reason can be found using
debugging, one can use AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
Best regards
igor