mmc_init fails in SPL of u-boot-boundary v2020.10 on nitrogen8m

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mmc_init fails in SPL of u-boot-boundary v2020.10 on nitrogen8m

1,198 次查看
colibri
Contributor I

Hi all,

 

I am using a nitrogen8m with u-boot-boundary v2020.10 (as used in meta-freescale-3rdparty's u-boot-boundary recipe). I want to access the mmc from within u-boot spl. However, already the mmc_init function fails. The error seems to occur in mmc_go_idle in driver/mmc/mmc.c which returns with -110. I would be glad if someone can point in into the right direction to find the cause.

 

Best regards

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,185 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Corinna

 

nitrogen8m is third party board developed and supported by its vendor : boundary devices.

One can recheck build steps on https://boundarydevices.com/u-boot-2020-10-for-i-mx-platforms/

and post issue to vendor support  https://boundarydevices.com/talk-with-an-engineer/

 

Best regards
igor

0 项奖励
回复