mmc_init fails in SPL of u-boot-boundary v2020.10 on nitrogen8m

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mmc_init fails in SPL of u-boot-boundary v2020.10 on nitrogen8m

1,222件の閲覧回数
colibri
Contributor I

Hi all,

 

I am using a nitrogen8m with u-boot-boundary v2020.10 (as used in meta-freescale-3rdparty's u-boot-boundary recipe). I want to access the mmc from within u-boot spl. However, already the mmc_init function fails. The error seems to occur in mmc_go_idle in driver/mmc/mmc.c which returns with -110. I would be glad if someone can point in into the right direction to find the cause.

 

Best regards

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,209件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Corinna

 

nitrogen8m is third party board developed and supported by its vendor : boundary devices.

One can recheck build steps on https://boundarydevices.com/u-boot-2020-10-for-i-mx-platforms/

and post issue to vendor support  https://boundarydevices.com/talk-with-an-engineer/

 

Best regards
igor

0 件の賞賛
返信