mipi_pll_div2_clk setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mipi_pll_div2_clk setting

Jump to solution
1,545 Views
pierluigi_p
Contributor V

Dear NXP experts,

according the Reference Manual of iMX8QXP (section 8.11.3.2, table 8-17), the MIPI DSI PLL has a fixed value of 864 MHz.

In the kernel dtsi, I can find the the declaration of mipi_pll_div2_clk as 432 MHz, half of the value declared in the Reference Manual.

Apparently, setting it to 864 MHz make no real changes: is this a fixed value because of a "div2" block ?

Given the mipi_pll_div2_clk at 432 MHz, which is the maximum display resolution for MIPI DSI ?

Thanks

Best Regards

Pier

Tags (1)
1 Solution
1,490 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @pierluigi_p 

mipi_pll_div2_clk:  clk is half of source pll.

You can find the maximum display resolution for MIPI DSI in datasheet.

  • Programmable display resolutions, from 160x120(QQVGA) to

    1920x1200(WUXGA) @ 60 fps, 24bpp

 

 

View solution in original post

0 Kudos
3 Replies
1,491 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @pierluigi_p 

mipi_pll_div2_clk:  clk is half of source pll.

You can find the maximum display resolution for MIPI DSI in datasheet.

  • Programmable display resolutions, from 160x120(QQVGA) to

    1920x1200(WUXGA) @ 60 fps, 24bpp

 

 

0 Kudos
1,475 Views
zee_z
Contributor III

Let us explore 1920x1080@60 Hz with RGB24.

display-timings {
    native-mode = <&timing0>;
    timing0: 1080p24 {
    /* 1920x1080p24 */
    clock-frequency = <52000000>;
    hactive = <1920>;
    vactive = <1080>;
    hfront-porch = <25>;
    hback-porch = <25>;
    hsync-len = <25>;
    vback-porch = <2>;
    vfront-porch = <2>;
    vsync-len = <2>;
    hsync-active = <1>;
};

(1920+25+25+25)x(1080+2+2+2)x60Hz = 1995x1086x60 = pclk 1299994200 MHz per lane (roughly 130 MHz).

Since we have simultaneously 4 lanes, to transport RGB24 we need 6 clocks, which gives us 130 MHz x 6 = 780 Mbit/s.

Roughly, 1920x1200 is around 792 Mbit/s < 800 MHz, defined per NXP as maximum MIPI DSI DPHY freq... Instead of 144 MHz x 6 = 864 MHz, as theoretical possibility, which NXP was never able to achieve due to the technology limitations.

Well!

Zoran
_______

0 Kudos
1,482 Views
pierluigi_p
Contributor V

Thanks @Zhiming_Liu !

Best Regards

Pier

0 Kudos