Hi everone,
My platform is IMX6Q-SDP and linux BSP version is L3.0.35_4.1.0_130816. Now I am testing Mini-PCIe wifi module(iwl4965) founction.
Support for iwl4965 is added in kernel driver.
A problem is that if I configure kernel like this:
Freescale MXC Implementations --->
PCI Express support
PCI Express EP mode in the IMX6 RC/EP interconnection system
PCI Express RC mode in the IMX6 RC/EP interconnection system
I can detect clock signal(100MHz) on pin11 and 13(REFCLK- and REFCLK+) during boot up. But they only lasts for about one secend
and then disappear.And PCIe link up failed:
If I configure like this:
Freescale MXC Implementations --->
PCI Express support
PCI Express EP mode in the IMX6 RC/EP interconnection system
PCI Express RC mode in the IMX6 RC/EP interconnection system
I can't get anly clock signal on those pins.
All the above can't make my pcie work and give the same error:
iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.
PCIE: imx_pcie_pltfm_probe start link up.
link up failed, DB_R0:0x00571600, DB_R1:0x08200000!
IMX PCIe port: link down!
Who can help me?
Hi, Xiaoqiang
clock signal(100MHz) on pins (REFCLK- and REFCLK+) is optional
signal, not all PCIe cards are using it. Freescale i.MX6 BSPs use
125MHz as this signal. You can add external 100MHz clock or try to find
card which does not require this signal. Some cards are mentioned
in Release Notes in Doc bundle, link below. Also please check
i.MX_6Dual6Quad_Linux_Reference_Manual.pdf
document sect.35.2.2 "Kernel configurations".
"L3.0.35_4.1.0_LINUX_DOCS "
Hi chipexpert,
My kernel is built acording to the manual, but it is of no help.Now I think something is wrong with the hardware.Because the pcie have been ok before and suddenly
broken down.So I will check my hardware. Thank you very much!