mic takes input from the ear pads/cushion in the headset not from the mic piece

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mic takes input from the ear pads/cushion in the headset not from the mic piece

1,237 Views
anushan
Contributor III

Hi Everyone,

I am facing a problem in recording from a headset mic on my imx8 m mini custom board. I am using wm8962 audio codec. The mic is taking input from the ear pads/cushion and not from the mic piece of the headset. I have a single audio jack in my hardware. Is this a problem. Or what could be causing the issue.

Kindly help in finding a solution.

Regards,

Anusha

0 Kudos
Reply
1 Reply

1,205 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anusha

one can try settings described in Table 7-7. Audio Mixer controls

Linux Manual in Linux 5.4.3_1.0.0 Documentation

mxc_amix_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply