Hello, Using below mentioned gstreamer pipeline for image capturing,
gst-launch mfw_v4lsrc device=/dev/video0 queue-size=[2 | 3 | 4] ! fakesink -v
When mfw_v4lsrc queue-size property is set to value 3 or less, based on timestamp, got to know that the captured image are been discarded. It works fine with queue-size property value set to 4. Find the logs attached
Gstreamer version: 0.10.36
MFW_GST_V4LSRC_PLUGIN version: 4.0.2
Regards,
Gautham
Original Attachment has been moved to: gst_fakesink_log.zip
解決済! 解決策の投稿を見る。
Hello,
The following - in section “Finding the Buffer Leak” from the linked below –
may explain the issue :
“ […] v4l2src has a buffer pool of a fixed number of buffers which are recycled along
the whole pipeline lifetime. This means that if the pool runs out of buffers, it must
wait until a buffer is freed to write a new image to it.
If v4l2 buffers are not returning fast enough you will lose images waiting for them
to free.”
Embedded GStreamer Performance Tuning - RidgeRun Developer Connection
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
The following - in section “Finding the Buffer Leak” from the linked below –
may explain the issue :
“ […] v4l2src has a buffer pool of a fixed number of buffers which are recycled along
the whole pipeline lifetime. This means that if the pool runs out of buffers, it must
wait until a buffer is freed to write a new image to it.
If v4l2 buffers are not returning fast enough you will lose images waiting for them
to free.”
Embedded GStreamer Performance Tuning - RidgeRun Developer Connection
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for the reply and link.
So to keep up to 30 fps, it is clear that, need to configure queue-size property of v4lsrc plugin with value 4 or more.
Regards,
Gautham