mfloat-abi=hard in IMX6 use the LTIB, compiling with the arm-linux-gnueabihf-

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mfloat-abi=hard in IMX6 use the LTIB, compiling with the arm-linux-gnueabihf-

2,272件の閲覧回数
xiexp
Contributor I

My system is Ubuntu 12.04 32bit ,now i want to  have the ubuntu 12.04hf system by compiling with the arm-linux-gnueabihf-.

now there have some error.

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

1,846件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi xie

please look at attached files showing toolchains options.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,846件の閲覧回数
xiexp
Contributor I

HI,

there also the same problem ,it is report " arm-linux-gnueabihf-gcc: error: -mfloat-abi=soft and -mfloat-abi=hard may not be used together".can you give some suggest?

0 件の賞賛
返信

1,846件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

error: -mfloat-abi=soft and -mfloat-abi=hard

explains itself: you can use one option, not both.

0 件の賞賛
返信

1,846件の閲覧回数
xiexp
Contributor I

my demoboard is imx6q, using the L3.035_4.1.0_130816_source, my computer is ubuntu 12.04,32bit .Now i want to compile the armhf .and the problem coming .

0 件の賞賛
返信

1,846件の閲覧回数
xiexp
Contributor I

my configure is -O2 -march=armv7-a -mfpu=vfpv7 -mfloat-abi=hard .

there is not option,when carry on the cammad ./ltib -c ,then problem is coming.

0 件の賞賛
返信