mfgtools can not download images?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mfgtools can not download images?

764 Views
13660284951
Contributor III

my board soc is imx6q

and i download linux or ubuntu images,which is not success?

while run to "jump to os images",it recircle to load uboot again.

the mfg tools log below

Labels (2)
0 Kudos
Reply
2 Replies

696 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhou

for new board (or processor) recommended first to run ddr test and update Mfg Tool firmware
image with new ddr calibration coefficients found from test
i.MX 6/7 DDR Stress Test Tool  
Update coefficients in uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg and
rebuild Mfg Tool firmware (files in  ../firmware folder, fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot).

For rebuilding use sect.6.2 Manufacturing Tool, MFGTool attached Yocto Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

696 Views
13660284951
Contributor III

hi

whatever i do,from mfgtool to make sd as startmedia,

the log is still below and can not write image success

U-Boot 2009.08-dirty (Nov 27 2013 - 10:51:14)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Thermal sensor with ratio = 175
Temperature: 36 C, calibration data 0x5524c369
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]
Boot Device: SPI NOR
I2C: ready
DRAM: 1 GB


U-Boot 2009.08-dirty (Nov 27 2013 - 10:51:14)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Thermal sensor with ratio = 175
Temperature: 36 C, calibration data 0x5524c369
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]
Boot Device: SPI NOR
I2C: ready
DRAM: 1 GB


U-Boot 2009.08-dirty (Nov 27 2013 - 10:51:14)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Thermal sensor with ratio = 175
Temperature: 36 C, calibration data 0x5524c369
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]
Boot Device: SPI NOR
I2C: ready
DRAM: 1 GB


U-Boot 2009.08-dirty (Nov 27 2013 - 10:51:14)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Thermal sensor with ratio = 175
Temperature: 36 C, calibration data 0x5524c369
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]
Boot Device: SPI NOR
I2C: ready
DRAM: 1 GB


U-Boot 2009.08-dirty (Nov 27 2013 - 10:51:14)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Thermal sensor with ratio = 175
Temperature: 36 C, calibration data 0x5524c369
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]
Boot Device: SPI NOR
I2C: ready
DRAM: 1 GB

0 Kudos
Reply