mfgtool2: maximum size of file for UCL2 pipe command?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mfgtool2: maximum size of file for UCL2 pipe command?

614 次查看
mikaelj
Contributor I

Hi,

I want to stream a 3GB file using the pipe command:

<CMD state="Updater" type="push" body="pipe dd of=/dev/mmcblk0 bs=1M" file="files/image.raw">Sending</CMD>

But file sizes >1GB will always fail, even though /dev/mmcblk0 is a 4GB eMMC. This on an MX6S.

Where is the limit documented? How do I lift the limit? I need to send this data to the device.

0 项奖励
回复
0 回复数