mfgtool : Waiting for /dev/utp to appear

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mfgtool : Waiting for /dev/utp to appear

2,293 Views
florian_germain
Contributor II

I have a problem with my board imx6sxsabresd and BSP imx-yocto-L4.14.78_1.0.0_ga.

When i use ramfs provided in mfgtool package (L4.9.88_2.0.0_mfg-tool) i can program my sabresd board.

I compile mfgtool firmwares and it seems that my ramfs is not well builded.

Changing fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot by the files builded with Yocto, mfgtool stuck at this line : 

Freeing unused kernel memory: 1024K
Found New UDC: ci_hdrc.0
ci_hdrc.0 0
ffs.utp0
file system registered
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
run utp at /dev/usb-utp0/ep0
.
uuu fastboot client 1.0.0 [built read descriptors
Feb 1 2019 12:47:25]
Start initread strings
usb
write string
Start handle command
uuc /dev/utp
uuc 0.5 [built Feb 1 2019 12:47:25]
UTP: Waiting for /dev/utp to appear
configfs-gadget gadget: high-speed config #1: c

Can anyone help me ?

Today i can program my sabresd board with prebuild ramfs but with my futur custom boards, it will not be possible.

Regards,

Labels (1)
0 Kudos
2 Replies

1,587 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Latest L4.14.78 uses uuu instead mfg tool. Please, see the below guide of how to use the uuu tool. It says that is for the i.MX8, but all the i.MX6 families are supported.

i.MX 8 Universal Update Utility (UUU) Tools and Pins Tool 

Hope this information can help you.

Best Regards,

Diego. 

1,587 Views
anush_deekonda
Contributor I

Hi Adrian,

I am using Yocto Sumo version.

The kernel boots up on yocto setup but there is no /dev/utp device node in the rootfs.

1. what kernel configuration need to be done inorder to create "/dev/utp" at boot up?

2. Also what is the major minor numbers of /dev/utp device node.

i am trying "uuc /dev/utp" which is not working.

3. Also the MFG tool on windows gets disconnected on kernel boot up on the yocto setup.

Is this expected behavior before launching uuc /dev/utp?

Thank you,

Anush D.

#MFG

#FSL_UTP

0 Kudos