mfgtool 1.6.2.0322 fails when sending firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mfgtool 1.6.2.0322 fails when sending firmware

1,006 Views
emilpedersen
Contributor I

Dear all

 

When using the mfgtool 1.6.2.0322 to update the flash image on my iMX28 board, the process always fails at some random point during sending of firmware. The error message is "Updater Error 0xffffff (-1) -"

 

Attachments show the following:

  • Screenshot from mfgtool after failure
  • Debug log from device
  • Screenshot showing PC and OS
  • Screenshot showing HID driver

 

Does anyone have an idea what I need to do differently in order make this tool work?

 

Br.

Emil

Original Attachment has been moved to: log.txt.zip

Tags (3)
0 Kudos
1 Reply

846 Views
igorpadykov
NXP Employee
NXP Employee

Hi Emil

reason may be that mfg tool firmware should be rebuilt for new board

with updated ddr settings (in bootlets ../boot_prep/init-mx28.c). Steps are

described in attached Linux Guide sect.2.5 Building the Manufacturing Firmware

https://community.freescale.com/message/321913#321913

https://community.freescale.com/docs/DOC-1455

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos