mfg u-boot.imx for imx6q som - Yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mfg u-boot.imx for imx6q som - Yocto

1,878 次查看
tuyennguyen
Contributor I

I have a custom board based on Sabresd. Everything runs smoothly when we boot it from SD card with new firmware.

However we are trying to flash it into NAND using manufacturing tool (MFG), we make a custom recipe called linux-imx-mfgtool_3.14.38.bb  for our board and then bitbake fsl-image-mfgtool-initramfs. The build finished successfully but there is no u-boot.imx which is required by MFG tool. Please advice me how to generate this u-boot.imx. I am sorry I am new in this Yocto project.

Thanks a lot.

标签 (1)
0 项奖励
回复
1 回复

1,557 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Carrie

please look at attached i.MX6 BSP Porting Guide sect.1.2.1 Preparing the Code

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复