mfg-tool stuck on Sending partition shell

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mfg-tool stuck on Sending partition shell

1,222 次查看
adriaanswanepoe
Contributor I


We are using the mfg-tool to setup a custom board based on the iMX6Q.

We have built updated versions of the mfg U-Boot, kernel, root file system, and device tree for our HW.

The mfg-tool detects the board when powered up, sends U-Boot, kernel, rfs and dtb and successfully jumps to U-Boot.

U-Boot successfully starts the kernel and the mass storage device comes up.

When the mfg-tool tries to execute the push send for mksdcard_new.sh.tar (Sending partition shell) step but gets stuck with no debug on the device.

Any recommendations, ideas, debug I need to provide?

Thanks,

Adriaan

标签 (2)
0 项奖励
回复
1 回复

983 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Adriaan

if baord stucks with no debug this may be due to memory errors.

https://community.freescale.com/docs/DOC-105652

Also one can try to execute these commands from linux, as mfg tools just runs

small linux image.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复