mfg tool failed for android 4.4.3.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mfg tool failed for android 4.4.3.

1,068 次查看
thangameenaraje
Contributor II

Hi, everyone,

I am working in sololite platform  custom board.

now i downloaded kitkat 4.4.3  it has kernel 3.10.17. i want to flash  emmc .

first i tried with my sololite evk.

in evk there is no emmc so for sdcard  .

1. downloaded mfg tool for 4.4.3.

2. given list name cfg.ini as  SDCard-Android-IMX6SL-EVK.    , mmc=0,1(tried both)

3. using sd2 slot inserted sd card. changed download mode.

4. added img files under android/evk/<.img>

5. executed exe. found hid device

6. its running but failed at partitioning.

7. error as fdisk not regognized.

i read the android firmware document. in that the given document is same as like for 4.4.2 mfg tool. in this 4.4.3 the kernel is in device tree format. there are more changes in bsp.

there is no file to compile ram uboot and ram kernel

under uboot/ include/configs/< mx6sl_evk_mfg.h>

kernel/arch/arm/configs/ imx6_updater_defconfig

to compile ram uboot and ram kernel

kindly help me in this issue


标签 (1)
0 项奖励
回复
1 回复

854 次查看
saurabh206
Senior Contributor III

Hi

Have you change  the Boot mode switch for firmware update?

You should change "Boot Mode" switch.

Thanks

Saurabh

0 项奖励
回复