method to convert 16bits generic data(IPU_PIX_FMT_GENERIC_16) to RGB Format

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

method to convert 16bits generic data(IPU_PIX_FMT_GENERIC_16) to RGB Format

ソリューションへジャンプ
3,920件の閲覧回数
ayyappadasps
Contributor II

hi all,

           I am using ov2710 parallel camera and pixel format  used is IPU_PIX_FMT_GENERIC_16 .

          I am able to capture an image,but it NOT coming in RGB format.

           could please help me to find a way to convert generic 16 pixel format to rgb pixel format

ラベル(3)
1 解決策
3,410件の閲覧回数
navinars
Contributor III

Hi,

  You can convert it online using the website rawpixels.net. 

I looked through the product info for OV2710 and saw that it supports only 8/10 bit raw data format. You will have to configure which stream the camera outputs by tweaking the camera registers. Assuming you are capturing 10-bit data, I think the format you should use for capturing is 0x30314742  (BG10)  GitHub - avafinger/cap-v4l2: capture frames from CMOS camera ov5640 / ov8865 using V4l2 and OpenCV. The pixel format should be V4L2_PIX_FMT_SBGGR10.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,410件の閲覧回数
ayyappadasps
Contributor II

hi  igorpadykov;

Thnx for your valuable replay.

Is there any external software tool to convert RAW image to RGB image format

0 件の賞賛
返信
3,411件の閲覧回数
navinars
Contributor III

Hi,

  You can convert it online using the website rawpixels.net. 

I looked through the product info for OV2710 and saw that it supports only 8/10 bit raw data format. You will have to configure which stream the camera outputs by tweaking the camera registers. Assuming you are capturing 10-bit data, I think the format you should use for capturing is 0x30314742  (BG10)  GitHub - avafinger/cap-v4l2: capture frames from CMOS camera ov5640 / ov8865 using V4l2 and OpenCV. The pixel format should be V4L2_PIX_FMT_SBGGR10.

0 件の賞賛
返信
3,410件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ayyappadas 

unfortunately ipu does not support convertion generic/raw format to rgb as answered on

https://community.nxp.com/message/309833#309833

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------