memtool issue on imx7d sabre board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

memtool issue on imx7d sabre board

1,271件の閲覧回数
akashgajjar
Contributor V

Hello,

i am accessing the register address of uart controller using memtool, command works properly

but when when i am accessing the i2c controller memory address using memtool, board stuck and

not responding.

root@imx7dpulse:~# /unit_tests/memtool UART1.UCR1.TXDMAEN
SOC: i.MX7D
UART1    Addr:0x30860000
UART1.UCR1 Addr:0x30860080 Value:0x00000241 -
UART1.UCR1.TXDMAEN(3..3)   :0x0
Transmitter Ready DMA Enable.

root@imx7dpulse:~#

root@imx7dpulse:~# /unit_tests/memtool I2C1.I2CR.TXAK
SOC: i.MX7D

(and after that not able to enter any command)

Regards,

Akash

ラベル(1)
1 返信

980件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Akash

are you using latest  L4.1.15_1.2.0 BSP, only it officially supports i.MX7

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.2.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

may be useful to check

https://community.nxp.com/thread/435782

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------