matchbox-keyboard - virtual keyboard loses focus in a web browser “password” field

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

matchbox-keyboard - virtual keyboard loses focus in a web browser “password” field

2,833件の閲覧回数
flaviosuligoi
Contributor IV

Hi all,

I'm using matchbox-keyboard, as virtual keyboard, in a HMI panel, based on i.MX53 architecture.

The distro (sato) is built using Yocto.

Normally the matchbox-keyboard (used as a daemon) works well, but when I try to write a password in a password field in a web page (ad example for a login), the matchbox-keyboard disappears.

This happens with both Chromium and Firefox.

If the browser works in "kiosk" mode, this is a big problem (in kiosk mode there is no status bar of the matchbox-desktop).

Any idea to solve this problem?

Thanks and best regards,

Flavio

0 件の賞賛
返信
3 返答(返信)

1,988件の閲覧回数
flaviosuligoi
Contributor IV

Nobody in Freescale has this problem like me?

Are nobody using Yocto to build kiosk-application with a web browser?

Flavio

0 件の賞賛
返信

1,988件の閲覧回数
davidlockyer
Contributor I

Hi Flavio,

Did you resolve your issue on this? If so, what steps did you need to take?

I noticed in another post (yocto mailing list) you had issues with the auto pop up in yocto 1.6.1? I am using yocto 1.6.4 and can't get the pop up working... My application is using chromium in kiosk mode.

Any advice would be much appreciated!

David

0 件の賞賛
返信

1,988件の閲覧回数
flaviosuligoi
Contributor IV

Nobody in Freescale has this problem like me?

Are nobody using Yocto to build kiosk-application with a web browser?

Flavio

0 件の賞賛
返信