main differences between Linux and winCE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

main differences between Linux and winCE

1,453 次查看
mv_shishkov
Contributor II

Could you tell me all main differences (licence, easy interchanging with processors, etc.) between Linux and winCE?

3 回复数

1,326 次查看
mv_shishkov
Contributor II

thank you very much

0 项奖励
回复

1,326 次查看
jamesbone
NXP TechSupport
NXP TechSupport

There are many differences  between both Operating Systems since always have been consider the opositive one from another, let try to  give you a comparation :

WINCE
Linux
All distributions has a cost in their LicenseAll distributions are for FREE
MIcrosoft Support Direct under some CostCommunity Support by FREE
Interchangeability only for Support Processors from MicrosoftBasically all Architecture of Processors are Supported and easy to build with MAKE file Cross Compiling supported
Multimedia Packages under DirectXA lot of different option of Frameworks, freescale use GSTREAMER
Codecs need to be compatible with DirectXCODEC support by the Framework.
Drivers review and approved by Microsoft less possible of bug since more deep testingDrivers provided by the Linux Community many people testing and contributing not an allign testing official process.

Let me know if you have another question


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,326 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Maksim,

You can go to google search for help:smileyhappy:~~
Have a great day,

Best Regards

Dan

0 项奖励
回复