machine name for imx6 dual wandboard in fsl-release-bsp 3.14 kernel?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

machine name for imx6 dual wandboard in fsl-release-bsp 3.14 kernel?

1,420 次查看
gbiradar
Contributor IV

Hi Guy

I'm using wandboard iMX6Dual development board, i have git repository i'm following freescale project user guide, Rev 0, 12/2015.

In section 5.1 Build configurations,

i have build yocto setup against imx6d machine but as i see in meta-fsl-arm/conf/machine i don't see imx6dual but rather solo/duallite/quad.

i need to know which machine configuration i can use for my project.

regards,

Ganesh

标签 (3)
标记 (2)
0 项奖励
回复
1 回复

1,212 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh

nxp linux documentation describes nxp reference boards, board

vendors may customize own bsps according to own boards configurations,

please follow wandboard guidelines:

Getting started with Yocto on Wandboard - Wandboard Wiki 

below common description of other vendors board support

difference between Yocto Community BSP and Free... | NXP Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复