hi
i am using a sabresd board,my lvds resolution ratio is 1440*540,my camera is ov5642;
when i run the Qt app,the lvds works fine;
but when i run the lvds test program,i got some confusion,i have test the following commands :
1 /unit_tests/mxc_v4l2_overlay.out -iw 1280 -ih 720 -ow 1024 -oh 480 -m 0 -di /dev/video0 -bg
2 /unit_tests/mxc_v4l2_overlay.out -iw 1280 -ih 720 -ow 1280 -oh 480 -m 0 -di /dev/video0 -bg
the first command result: the screen show 1024*480 picture size from the camera capture,so it is right;
the second commandresult: the screen show a full screen picture size from the camera capture,i only want a 1280*408 output image,why it show a full screen;
then i used the hdmi monitor to take the same test,the result is as above;
conclusion:
it seems that
when i set the output width less than 1024,the output image is just the right size as i had set;
when i set the output width greater than 1024,the output image will be the seem size as the full screen,it is not what i want;
it should be not right,when i want the output image width size greater than 1024,but not a full screen size,how to make the right set;
i am looking forward to your reply,and thank you very much
Hi Cheng
some IPU operations have the limit of 1024x1024 as explained on
https://community.nxp.com/message/361253?commentID=361253#comment-361253
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------