lvds display on i.MX 6Quad android 4.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lvds display on i.MX 6Quad android 4.2

ソリューションへジャンプ
5,375件の閲覧回数
tonnywong
Contributor III

Hi,All.

I try to use lvds display on  sabre-sd board (i.MX 6Quad), Android 4.2.2_1, but the display is not correct ,both the resolution and color is not right :


Home.jpg


apps.jpg

the panel is LP101WX1-SLN2 from LG , its specification is:

panel.JPG.jpg

I folow the below steps to port the display driver:

1. connect the hardware between the panel and board through lvds1


2. modify fb_videomode variable of kernel drivers/video/mxc/ldb.c:

--------------------------------------------------------------------

static struct fb_videomode ldb_modedb[] = {

  {

   "LDB-WXGA", 60, 1280, 800, 14065,

   40, 40,

   10, 3,

   80, 10,

   0,

   FB_VMODE_NONINTERLACED,

   FB_MODE_IS_DETAILED,},

   {

     "LDB-XGA", 60, 1280, 800, 14430,

     80, 48,

     15, 2,

     32, 47,

     0,

     FB_VMODE_NONINTERLACED,

     FB_MODE_IS_DETAILED,},

  {

   "LDB-1080P60", 60, 1920, 1080, 7692,

   100, 40,

   30, 3,

   10, 2,

   0,

   FB_VMODE_NONINTERLACED,

   FB_MODE_IS_DETAILED,},

};

i change the 'LDB-XGA‘ member's parameters refer to my panel:

1)name is LDB-XGA

2)refresh is 60

3)resolution is 1280*800

4)clock is 10^12/(69.3*10^6)=14430

5)left_margin=80, right_margin=48, upper_margin=15 , lower_margin=2

6)hsync_len=32 , vsync_len=47

3. build and  run the jb4.2.2_1 system, set bootargs below :

setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 vmalloc=400M init=/init video=mxcfb0:dev=ldb video=mxcfb1:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb2:off fbmem=10M androidboot.hardware=freescale

After it boots up, the lvds display appears not normal as I said at the start ,but the hdmi display is ok.



I've try several ways to resolve this problem, but none of it work.

1)edit fb_videomode variable of u-boot-imx/board/freescale/mx6q_sabresd.c ,make it the same as ldb.c of kernel:

{

   " XGA", 60, 1280, 800, 14430,

   80, 48,

   15, 2,

   32, 47,

   0,

   FB_VMODE_NONINTERLACED,

   FB_MODE_IS_DETAILED,

}

2)change bootargs like: video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666,bpp=16 video=mxcfb1:off video=mxcfb2

...

Finally, I download android 4.0.4 source ,andr patch imx-android-r13.4.1 , and modify fb_videomode  variable of ldb.c (the same as I said before),  build and run the system, the lvds display's resolution is correct , and  the color is better:

C360_2013-08-13-12-26-22-457.jpg

So the display on android 4.0.4 is ok, but for android 4.2.2_1 is not ok,both base on the same sabre-sd board and display panel.

Can anyone tell me, how to resolve this problem on android 4.2.2_1, just make correct resolution of lvds display?

ラベル(4)
0 件の賞賛
返信
1 解決策
3,324件の閲覧回数
tonnywong
Contributor III

Hi,All.

I've find the reason, the color issue is caused by lvds cable, after i change a better lvds cable, the colour becomes normal.

Thanks all.

元の投稿で解決策を見る

0 件の賞賛
返信
10 返答(返信)
3,324件の閲覧回数
tonnywong
Contributor III

The resolution problem on android 4.2.2_1 is fixed now, i add 'bpp=32' at bootargs like:

setenv bootargs console=ttymxc0,115200 androidboot.console=ttymxc0 vmalloc=400M init=/init video=mxcfb0:dev=ldb, bpp=32 video=mxcfb1:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb2:off fbmem=10M androidboot.hardware=freescale



but the color of display is not right, like photos below:

20130820_092019.jpg

20130820_092447.jpg

20130820_092420.jpg



I think it's due to the 'bpp=32', my display panel is 18 bit of 3 pairs of data signals, so when using bpp=32 get correct resolution but wrong color.

if someone konw, please tell me how to do fo resolve this color problem, thanks.

3,325件の閲覧回数
tonnywong
Contributor III

Hi,All.

I've find the reason, the color issue is caused by lvds cable, after i change a better lvds cable, the colour becomes normal.

Thanks all.

0 件の賞賛
返信
3,324件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Have you try "video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666,bpp=32" ?

3,324件の閲覧回数
tonnywong
Contributor III

Thanks for your reply, the resolution is ok when adding 'bpp=32', but the color still not right as showed in adjacent post.

0 件の賞賛
返信
3,324件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Please try to increase the fbmem.

The reserved Framebuffer size is configured through boot parameters "fbmem=nM" in U-Boot. The formula to calculate "n" is shown below:

n= width * height * buffer_number * sizeof(format)

Width is the width of the display panel by pixel.

Height is the height of the display panel by pixel.

buffer_number is the number of buffers for Framebuffer0. The default value is 3.

sizeof (format) is the size of each pixel of specific format by bytes. For 16bpp, sizeof (format) is 2 bytes. For 32bpp, the sizeof (32bpp) is 4 bytes.

0 件の賞賛
返信
3,324件の閲覧回数
tonnywong
Contributor III

Hi, jimmy.

According to my panel , fbmen=1280*800*3*4B=12MB, I've try fbmem=12M or 64M, it doesn't seem to work.

0 件の賞賛
返信
3,324件の閲覧回数
LeviathanSteven
Contributor III

Hi,

According to function mxcfb_option_setup, maybe you can try "video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666,bpp=24" ?

0 件の賞賛
返信
3,324件の閲覧回数
tonnywong
Contributor III

I've try bpp=24 or 16, they would cause the resolution and color problem as showed at the start of topic.

Only bpp=32 can get correct resolution, but it's color is not right as showed at my second post.

0 件の賞賛
返信
3,324件の閲覧回数
varsmolta
Contributor V

check the bootargs of the android 4.0.4 vs the android 4.2.2_1 versions for the u-boot. Are they different? Look for when the kernel boots. The bootargs should be in the log at the beginning of the kernel booting.

Also, you can use the "fbset -t" and/or "fbset --move" and use trial and error to get the timing params that will work with your lvds display.

0 件の賞賛
返信
3,324件の閲覧回数
tonnywong
Contributor III

thanks for you reply, the resolution is ok when adding 'bpp=32' to bootargs.

0 件の賞賛
返信