ltib "mfg firmware profile" build error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ltib "mfg firmware profile" build error

1,191 次查看
sangjinhong
Contributor III

ltib "min profile" build ssuccessful.

However, "mfg firmware profile" failed.

The following is error message.

Could anybody let know why???

=================== error message =================

+ [ /home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08 != /home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08 ]

+ cd /home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08

+ [ -n  ]

+ make HOSTCC=ccache /usr/bin/gcc -B/usr/bin/ CROSS_COMPILE=arm-none-linux-gnueabi- O=/home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08 mx6dl_sabresd_mfg_config

make: *** No rule to make target `mx6dl_sabresd_mfg_config'.  Stop.

error: Bad exit status from /home/john/dev/freescale/dev_env/ltib/tmp/rpm-tmp.23807 (%build)

RPM build errors:

    Bad exit status from /home/john/dev/freescale/dev_env/ltib/tmp/rpm-tmp.23807 (%build)

Build time for u-boot-v2009.08: 0 seconds

Failed building u-boot-v2009.08

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Wed Feb  5 15:09:11 2014

Ended:   Wed Feb  5 15:09:14 2014

Elapsed: 3 seconds

These packages failed to build:

u-boot-v2009.08

Build Failed

Exiting on error or interrupt

标签 (1)
0 项奖励
回复
1 回复

1,046 次查看
sangjinhong
Contributor III

There are my mistakes.

0 项奖励
回复