ltib "mfg firmware profile" build error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ltib "mfg firmware profile" build error

1,240件の閲覧回数
sangjinhong
Contributor III

ltib "min profile" build ssuccessful.

However, "mfg firmware profile" failed.

The following is error message.

Could anybody let know why???

=================== error message =================

+ [ /home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08 != /home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08 ]

+ cd /home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08

+ [ -n  ]

+ make HOSTCC=ccache /usr/bin/gcc -B/usr/bin/ CROSS_COMPILE=arm-none-linux-gnueabi- O=/home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08 mx6dl_sabresd_mfg_config

make: *** No rule to make target `mx6dl_sabresd_mfg_config'.  Stop.

error: Bad exit status from /home/john/dev/freescale/dev_env/ltib/tmp/rpm-tmp.23807 (%build)

RPM build errors:

    Bad exit status from /home/john/dev/freescale/dev_env/ltib/tmp/rpm-tmp.23807 (%build)

Build time for u-boot-v2009.08: 0 seconds

Failed building u-boot-v2009.08

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Wed Feb  5 15:09:11 2014

Ended:   Wed Feb  5 15:09:14 2014

Elapsed: 3 seconds

These packages failed to build:

u-boot-v2009.08

Build Failed

Exiting on error or interrupt

ラベル(1)
0 件の賞賛
返信
1 返信

1,095件の閲覧回数
sangjinhong
Contributor III

There are my mistakes.

0 件の賞賛
返信