hi there,
i'm getting the following error while running ./ltib anyone help me
ltib cannot be run because one or more of the host packages needed to run it
are either missing or out of date or not in ltib's standard path. Please
install/upgrade these packages on your host. If you have your own utilities
in non-standard paths, please add an entry into the .ltibrc file for example:
%path_std
/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes
Package Minimum ver Installed info
------- ----------- ---------------
zlib 0 not installed
Died at ./ltib line 1409.
traceback:
main::host_checks:1409
main:554
Started: Sun Oct 18 11:13:59 2015
Ended: Sun Oct 18 11:14:02 2015
Elapsed: 3 seconds
Build Failed
Exiting on error or interrupt
Hello Sarathkumar Natarajan,
I would suggest reviewing the following thread which talks about this same issue.