ltib imx53 qsb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib imx53 qsb

415 Views
didier1
Contributor I

Hi,

If i use the image for the SD on a QSB start-r, i can use usb_modeswitch, modem-manager and some other command (like "service"..).

When i compile the source with ltib, this command are not present, how to retrieve them?

Thanks for help

Seize

Labels (2)
0 Kudos
1 Reply

358 Views
igorpadykov
NXP Employee
NXP Employee

Hi seize

one can backport these software packages, if they are

not available in ltib packages selection. Guidelines for adding

custom application to ltib can be found in i.MX PDK Linux Application Note

"Hello World" in Doc package

Supporting Information (4)

i.MX25 SDK 2009.12 Linux Documentation Bundle (REV 2009.12)

http://www.nxp.com/products/interface-and-connectivity/interface-and-system-management/switch-monito...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos