ltib imx28 fails with fontconfig

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib imx28 fails with fontconfig

Jump to solution
2,113 Views
Davros
Contributor III

Greetings,

I am trying to build imx28 FSL gnome package for imx28 EVK board.  I have downloaded the following:

L2.6.35_10.12.01_SDK_source.tar.gz

I am running Ubuntu 10.04, 64 bit:

$ cat /etc/lsb-release

DISTRIB_ID=Ubuntu

DISTRIB_RELEASE=10.04

DISTRIB_CODENAME=lucid

DISTRIB_DESCRIPTION="Ubuntu 10.04.4 LTS"

I have extracted the source package, and ran the install.  I configured ltib for FSL gnome package, and changed the target hostname.  After exiting, the build run run for a while, but then fail.  If I do the following, it will fail the same way:

$ ./ltib -p fontconfig

Processing platform: Freescale iMX28 Based Boards

===================================================

using config/platform/imx/.config

Processing: fontconfig

========================

Build path taken because: no prebuilt rpm,

rpmbuild --dbpath /opt/freescale_imx28/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /opt/freescale_imx28/ltib/rpm' --define '_prefix /usr' --define '_tmppath /opt/freescale_imx28/ltib/tmp' --define '_rpmdir /opt/freescale_imx28/ltib/rpm/RPMS'  --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bb --clean --rmsource  /opt/freescale_imx28/ltib/dist/lfs-5.1/fontconfig/fontconfig.spec

Building target platforms: arm

Building for target arm

Executing(%prep): /bin/sh -e /opt/freescale_imx28/ltib/tmp/rpm-tmp.94447

+ umask 022

+ cd /opt/freescale_imx28/ltib/rpm/BUILD

+ cd /opt/freescale_imx28/ltib/rpm/BUILD

+ rm -rf fontconfig-2.4.2

+ /bin/gzip -dc /opt/freescale_imx28/ltib/rpm/SOURCES/fontconfig-2.4.2.tar.gz

+ tar -xvvf -

drwxrwxrwx 1488/100          0 2006-12-02 17:32 fontconfig-2.4.2/

drwxrwxrwx 1488/100          0 2006-12-02 17:32 fontconfig-2.4.2/doc/

.... [removing file list from rpm]

-rw-rw-r-- 1488/100       1640 2006-09-03 17:37 fontconfig-2.4.2/test/run-test.sh

-rw-rw-r-- 1488/100      70952 2006-08-27 16:36 fontconfig-2.4.2/test/4x6.pcf

-rw-rw-r-- 1488/100      21320 2006-08-27 16:36 fontconfig-2.4.2/test/8x16.pcf

-rw-rw-r-- 1488/100        115 2006-08-27 16:36 fontconfig-2.4.2/test/out.expected

-rw-rw-r-- 1488/100         80 2006-09-03 17:37 fontconfig-2.4.2/test/fonts.conf.in

+ STATUS=0

+ [ 0 -ne 0 ]

+ cd fontconfig-2.4.2

+ exit 0

Executing(%build): /bin/sh -e /opt/freescale_imx28/ltib/tmp/rpm-tmp.94447

+ umask 022

+ cd /opt/freescale_imx28/ltib/rpm/BUILD

+ cd fontconfig-2.4.2

+ ac_cv_prog_HASDOCBOOK=no ac_cv_prog_CC_FOR_BUILD=ccache /usr/bin/gcc -B/usr/bin/ ./configure --prefix=/usr --host=arm-linux --build=x86_64-unknown-linux-gnu --with-arch=arm --sysconfdir=/etc

checking for a BSD-compatible install... /usr/bin/install -c

checking whether build environment is sane... yes

checking for gawk... gawk

checking whether make sets $(MAKE)... yes

checking for arm-linux-strip... arm-linux-strip

checking whether to enable maintainer-specific portions of Makefiles... no

checking for arm-linux-gcc... gcc

checking for C compiler default output file name... a.out

checking whether the C compiler works... yes

checking whether we are cross compiling... yes

checking for suffix of executables...

checking for suffix of object files... o

checking whether we are using the GNU C compiler... yes

checking whether gcc accepts -g... yes

checking for gcc option to accept ISO C89... none needed

checking for style of include used by make... GNU

checking dependency style of gcc... gcc3

checking for a BSD-compatible install... /usr/bin/install -c

checking whether ln -s works... yes

checking build system type... x86_64-unknown-linux-gnu

checking host system type... arm-unknown-linux-gnu

checking for a sed that does not truncate output... /bin/sed

checking for grep that handles long lines and -e... /bin/grep

checking for egrep... /bin/grep -E

checking for ld used by gcc... ld

checking if the linker (ld) is GNU ld... yes

checking for ld option to reload object files... -r

checking for BSD-compatible nm... /opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-linux-nm -B

checking how to recognise dependent libraries... pass_all

checking how to run the C preprocessor... gcc -E

checking for ANSI C header files... yes

checking for sys/types.h... yes

checking for sys/stat.h... yes

checking for stdlib.h... yes

checking for string.h... yes

checking for memory.h... yes

checking for strings.h... yes

checking for inttypes.h... yes

checking for stdint.h... yes

checking for unistd.h... yes

checking dlfcn.h usability... yes

checking dlfcn.h presence... yes

checking for dlfcn.h... yes

checking whether we are using the GNU C++ compiler... yes

checking whether g++ accepts -g... yes

checking dependency style of g++... gcc3

checking how to run the C++ preprocessor... g++ -E

checking for arm-linux-g77... no

checking for arm-linux-f77... no

checking for arm-linux-xlf... no

checking for arm-linux-frt... no

checking for arm-linux-pgf77... no

checking for arm-linux-cf77... no

checking for arm-linux-fort77... no

checking for arm-linux-fl32... no

checking for arm-linux-af77... no

checking for arm-linux-f90... no

checking for arm-linux-xlf90... no

checking for arm-linux-pgf90... no

checking for arm-linux-pghpf... no

checking for arm-linux-epcf90... no

checking for arm-linux-gfortran... no

checking for arm-linux-g95... no

checking for arm-linux-f95... no

checking for arm-linux-fort... no

checking for arm-linux-xlf95... no

checking for arm-linux-ifort... no

checking for arm-linux-ifc... no

checking for arm-linux-efc... no

checking for arm-linux-pgf95... no

checking for arm-linux-lf95... no

checking for arm-linux-ftn... no

checking for g77... no

checking for f77... no

checking for xlf... no

checking for frt... no

checking for pgf77... no

checking for cf77... no

checking for fort77... no

checking for fl32... no

checking for af77... no

checking for f90... no

checking for xlf90... no

checking for pgf90... no

checking for pghpf... no

checking for epcf90... no

checking for gfortran... no

checking for g95... no

checking for f95... no

checking for fort... no

checking for xlf95... no

checking for ifort... no

checking for ifc... no

checking for efc... no

checking for pgf95... no

checking for lf95... no

checking for ftn... no

checking whether we are using the GNU Fortran 77 compiler... no

checking whether  accepts -g... no

checking the maximum length of command line arguments... 32768

checking command to parse /opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-linux-nm -B output from gcc object... ok

checking for objdir... .libs

checking for arm-linux-ar... ar

checking for arm-linux-ranlib... arm-linux-ranlib

checking for arm-linux-strip... (cached) arm-linux-strip

checking if gcc supports -fno-rtti -fno-exceptions... no

checking for gcc option to produce PIC... -fPIC

checking if gcc PIC flag -fPIC works... yes

checking if gcc static flag -static works... yes

checking if gcc supports -c -o file.o... rmdir: failed to remove `conftest': Directory not empty

rm: cannot remove `conftest': Is a directory

yes

checking whether the gcc linker (ld) supports shared libraries... yes

checking whether -lc should be explicitly linked in... rm: cannot remove `conftest': Is a directory

rm: cannot remove `conftest': Is a directory

no

checking dynamic linker characteristics... GNU/Linux ld.so

checking how to hardcode library paths into programs... immediate

checking whether stripping libraries is possible... yes

checking if libtool supports shared libraries... yes

checking whether to build shared libraries... yes

checking whether to build static libraries... yes

configure: creating libtool

appending configuration tag "CXX" to libtool

rm: cannot remove `conftest': Is a directory

rm: cannot remove `conftest': Is a directory

checking for ld used by g++... ld

checking if the linker (ld) is GNU ld... yes

checking whether the g++ linker (ld) supports shared libraries... yes

checking for g++ option to produce PIC... -fPIC

checking if g++ PIC flag -fPIC works... rm: cannot remove `conftest': Is a directory

yes

checking if g++ static flag -static works... rm: cannot remove `conftest': Is a directory

no

checking if g++ supports -c -o file.o... rmdir: failed to remove `conftest': Directory not empty

rm: cannot remove `conftest': Is a directory

yes

checking whether the g++ linker (ld) supports shared libraries... yes

checking dynamic linker characteristics... GNU/Linux ld.so

checking how to hardcode library paths into programs... immediate

appending configuration tag "F77" to libtool

checking whether make sets $(MAKE)... (cached) yes

checking for a C compiler for build tools... checking for gcc... (cached) ccache /usr/bin/gcc -B/usr/bin/

ccache /usr/bin/gcc -B/usr/bin/

checking for suffix of executable build tools... rm: cannot remove `conftest': Is a directory

configure: error: Cannot determine suffix of executable build tools

error: Bad exit status from /opt/freescale_imx28/ltib/tmp/rpm-tmp.94447 (%build)

RPM build errors:

    Bad exit status from /opt/freescale_imx28/ltib/tmp/rpm-tmp.94447 (%build)

Build time for fontconfig: 6 seconds

Failed building fontconfig

f_buildrpms() returned an error, exiting

traceback:

main:560

Started: Mon Feb  4 15:28:56 2013

Ended:   Mon Feb  4 15:29:02 2013

Elapsed: 6 seconds

These packages failed to build:

fontconfig

Build Failed

Exiting on error or interrupt

I am a bit concerned over the "--build=x86_64-unknown-linux-gnu" option in the fontconfig configuration option, although I am not sure what it should be set to, or even how to change it.

Daryl

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
1,322 Views
Davros
Contributor III

This has been resolved.  The particular shell I was using had an Android build environment setup in it, which seemingly does work well with ltib environment.    If having build problems, check the shell environment.

Sorry for your trouble.

Daryl

View solution in original post

0 Kudos
Reply
3 Replies
1,323 Views
Davros
Contributor III

This has been resolved.  The particular shell I was using had an Android build environment setup in it, which seemingly does work well with ltib environment.    If having build problems, check the shell environment.

Sorry for your trouble.

Daryl

0 Kudos
Reply
1,322 Views
gagangarg
Contributor II

Hello Daryl,

I have also encountered the same problem while building.

I have checked my environment and it is bash.

Still it is not working.

I am not able to get the reason of it.

Regards

Gagan

0 Kudos
Reply
1,322 Views
Davros
Contributor III

Hi Gagan,

I am not exactly sure what the problem was, paths to incorrect compiler and components were likely.  However, I do use the following environment setup script from a base login shell:

----------------------------------------

if [ -z "$ZSH_NAME" ] && [ "x$0" = "x./environment-setup" ]; then

    echo "Error: This needs sourced. Please run as \". ./environment-setup\""

    exit 1

else

    if [ -n "$BASH_SOURCE" ]; then

        SDK_PATH="`dirname $BASH_SOURCE`"

    else

        SDK_PATH="`pwd`"

    fi

    SDK_PATH=`readlink -f "$SDK_PATH"`

    export SDK_PATH=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi

fi

export TOOLCHAIN_PATH=$SDK_PATH

export TARGET_SYS=arm-fsl-linux-gnueabi

export PATH=$SDK_PATH/bin:$TOOLCHAIN_PATH/bin:$PATH

export CPATH=$SDK_PATH/$TARGET_SYS/usr/include:$CPATH

export LIBTOOL_SYSROOT_PATH=$SDK_PATH/$TARGET_SYS

export PKG_CONFIG_SYSROOT_DIR=$SDK_PATH/$TARGET_SYS

export CC=arm-fsl-linux-gnueabi-gcc

export CPP="arm-fsl-linux-gnueabi-gcc -E"

export NM=arm-fsl-linux-gnueabi-nm

export RANLIB=arm-fsl-linux-gnueabi-ranlib

export OBJCOPY=arm-fsl-linux-gnueabi-objcopy

export STRIP=arm-fsl-linux-gnueabi-strip

export AS=arm-fsl-linux-gnueabi-as

export AR=arm-fsl-linux-gnueabi-ar

export OBJDUMP=arm-fsl-linux-gnueabi-objdump

export CROSS_COMPILE=arm-fsl-linux-gnueabi-

export ARCH=arm

-----------------------------------------------------------------------------------------------

Notice my placement of the arm-fsl cross compiler.  As far as ltib itself goes, I think Freescale only tests two of the available build profiles, the base one and the full Gnome profile.  I am not sure what will work outside of those two.

For completeness, I'll include my full environment so you might be able to match and compare what the problem might well be:

------------------------------------------------------------------

$ printenv

AS=arm-fsl-linux-gnueabi-as

AR=arm-fsl-linux-gnueabi-ar

SSH_AGENT_PID=1448

TERM=xterm

SHELL=/bin/bash

NM=arm-fsl-linux-gnueabi-nm

WINDOWID=73421175

OLDPWD=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0

GTK_MODULES=canberra-gtk-module

USER=daryl

PKG_CONFIG_SYSROOT_DIR=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/arm-fsl-linux-gnueabi

TOOLCHAIN_PATH=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi

CPATH=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/arm-fsl-linux-gnueabi/usr/include:

DEFAULTS_PATH=/usr/share/gconf/gnome.default.path

USERNAME=daryl

CPP=arm-fsl-linux-gnueabi-gcc -E

XDG_CONFIG_DIRS=/etc/xdg/xdg-gnome:/etc/xdg

TARGET_SYS=arm-fsl-linux-gnueabi

DESKTOP_SESSION=gnome

PATH=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin:/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin:/home/daryl/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/home/daryl/bin

PWD=/opt/freescale

STRIP=arm-fsl-linux-gnueabi-strip

GDM_KEYBOARD_LAYOUT=us

LANG=en_US.UTF-8

MANDATORY_PATH=/usr/share/gconf/gnome.mandatory.path

GDM_LANG=en_US.UTF-8

GDMSESSION=gnome

OBJCOPY=arm-fsl-linux-gnueabi-objcopy

SPEECHD_PORT=7560

SHLVL=1

HOME=/home/daryl

SDK_PATH=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi

GNOME_DESKTOP_SESSION_ID=this-is-deprecated

LOGNAME=daryl

XDG_DATA_DIRS=/usr/share/gnome:/usr/local/share/:/usr/share/

DBUS_SESSION_BUS_ADDRESS=unix:abstract=/tmp/dbus-UFruqpg5uP,guid=3e70a9c87dfb0f118ebd7d17515036f4

LESSOPEN=| /usr/bin/lesspipe %s

USE_CCACHE=1

ARCH=arm

RANLIB=arm-fsl-linux-gnueabi-ranlib

LIBTOOL_SYSROOT_PATH=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/arm-fsl-linux-gnueabi

CROSS_COMPILE=arm-fsl-linux-gnueabi-

CC=arm-fsl-linux-gnueabi-gcc

DISPLAY=:0.0

OBJDUMP=arm-fsl-linux-gnueabi-objdump

LESSCLOSE=/usr/bin/lesspipe %s %s

COLORTERM=gnome-terminal

_=/usr/bin/printenv

--------------------------------------------------------------------------------

I hope this helps, and good luck.

Daryl

0 Kudos
Reply