ltib for imx51 board - ltib error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ltib for imx51 board - ltib error

1,214 次查看
computer996633
Contributor I

fsl_shw_rand.c:46:24: error: shw_driver.h: No such file or directory
fsl_shw_rand.c:49: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'validate_uco'
fsl_shw_rand.c:56: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'fsl_shw_get_random'
fsl_shw_rand.c:84: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'fsl_shw_add_entropy'
make[1]: *** [fsl_shw_rand.o] Error 1
make[1]: Leaving directory `/home/auto/Varadharajan/YBV/L2.6.31_09.12.00_SDK_source/Nov16/ltib/rpm/BUILD/imx-lib-09.12.00/rng'
make: *** [rng] Error 2
error: Bad exit status from /home/auto/Varadharajan/YBV/L2.6.31_09.12.00_SDK_source/Nov16/ltib/tmp/rpm-tmp.84200 (%build)


RPM build errors:
    Bad exit status from /home/auto/Varadharajan/YBV/L2.6.31_09.12.00_SDK_source/Nov16/ltib/tmp/rpm-tmp.84200 (%build)
Build time for imx-lib: 0 seconds

Failed building imx-lib


f_buildrpms() returned an error, exiting
traceback:
 main:560


Started: Thu Nov 17 12:36:37 2011
Ended:   Thu Nov 17 12:37:28 2011
Elapsed: 51 seconds

These packages failed to build:
imx-lib

Build Failed

标记 (1)
0 项奖励
回复
1 回复

815 次查看
KrishnaPavan
Contributor II

Hi, Varadharajan,

Were you able to resolve the error with the build, by now?

 

If not then,

Did you configure your ltib properly?

 

From your log it seems there is some problem with the configuration itself.

 

Regards Krishna Pavan

0 项奖励
回复