user@SYSTEM:~/imx28/ltib_31/ltib$ ./ltib
ltib cannot be run because one or more of the host packages needed to run it
are either missing or out of date or not in ltib's standard path. Please
install/upgrade these packages on your host. If you have your own utilities
in non-standard paths, please add an entry into the .ltibrc file for example:
%path_std
/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes
Package Minimum ver Installed info
------- ----------- ---------------
glibc-devel 0 not installed
zlib 0 not installed
Died at ./ltib line 1397.
traceback:
main::host_checks:1397
main:542
Started: Tue Apr 3 15:32:47 2018
Ended: Tue Apr 3 15:32:47 2018
Elapsed: 0 seconds
Build Failed
Exiting on error or interrupt
user@BLTSP01211:~/imx28/ltib_31/ltib$ which zlib
/usr/bin/zlib
user@BLTSP01211:~/imx28/ltib_31/ltib$ glib-
glib-compile-resources glib-compile-schemas glib-genmarshal glib-gettextize glib-mkenums
Please Help me to solve this issue?
Thanks in Advance!