ltib busybox build fail, fedora 15.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib busybox build fail, fedora 15.

1,944 Views
Ameeca
Contributor II

Hi all,

 

Will anyone help me solve this problem -

 

I'm building busybox into my ltib package list but keep coming up against the following. I know there are issues with the makefile in /opt/freescale/packages/busybox-1.15.0 but I don't know how to fix them.

[david@localhost ltib]$ ./ltib

Processing platform: Freescale iMX233/stmp3780 Based Boards
=============================================================
using config/platform/imx/.config

Processing: fake-provides
===========================

Processing: u-boot
====================

Processing: kernel-2.6.31
===========================

Processing: skell
===================

Processing: base_libs
=======================

Processing: busybox
=====================
Build path taken because: directory build, no prebuilt rpm,
scbuild/scdeploy already unpacked package

Processing: busybox
=====================
Build path taken because: directory build, build key set, no prebuilt rpm,

rpmbuild --dbpath /home/david/Freescale/new/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/david/Freescale/new/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/david/Freescale/new/ltib/tmp' --define '_rpmdir /home/david/Freescale/new/ltib/rpm/RPMS'  --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit  /home/david/Freescale/new/ltib/dist/lfs-5.1/busybox/busybox.spec
Building target platforms: arm
Building for target arm
Executing(%build): /bin/sh -e /home/david/Freescale/new/ltib/tmp/rpm-tmp.27768
+ umask 022
+ cd /home/david/Freescale/new/ltib/rpm/BUILD
+ cd busybox-1.15.0
+ PKG_BUSYBOX_PRECONFIG=busybox.config
+ '[' -f /home/david/Freescale/new/ltib/config/platform/imx/busybox.config ']'
+ cp /home/david/Freescale/new/ltib/config/platform/imx/busybox.config .config
+ '[' -n '' -o -n '' ']'
+ yes ''
+ make config 'HOSTCC=ccache /usr/bin/gcc -B/usr/bin/'
Makefile:1270: *** mixed implicit and normal rules.  Stop.
error: Bad exit status from /home/david/Freescale/new/ltib/tmp/rpm-tmp.27768 (%build)


RPM build errors:
    Bad exit status from /home/david/Freescale/new/ltib/tmp/rpm-tmp.27768 (%build)
Build time for busybox: 0 seconds

Failed building busybox


f_buildrpms() returned an error, exiting
traceback:
 main:560


Started: Mon Oct 17 14:20:43 2011
Ended:   Mon Oct 17 14:20:44 2011
Elapsed: 1 seconds

These packages failed to build:
busybox

Build Failed

Tags (1)
0 Kudos
Reply
3 Replies

1,447 Views
Nagraj
Contributor I
The above mentioned change is not working still the same output is repeating? Thanks in advance.
0 Kudos
Reply

1,447 Views
Ameeca
Contributor II

Thanks Patrick. As I said I'm aware the Makefile needs changing. When I attepmt to save the file and update the archive, an error occurs and the archive will no longer load;

 

/bin/gtar: Skipping to next header.

/bin/gtar: Exiting with failure status due to previous error.

 

Patrick Chau said:

HI 

     Edit the Makefile for busybox, change:

 

        line 1270:  / %/: prepare scripts FORCE

 

     to 

        line 1270:   %/: prepare scripts FORCE

 

Patrick

0 Kudos
Reply

1,446 Views
PatrickChau
Contributor II

HI 

     Edit the Makefile for busybox, change:

 

        line 1270:  / %/: prepare scripts FORCE

 

     to 

        line 1270:   %/: prepare scripts FORCE

 

Patrick

0 Kudos
Reply