ltib build error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ltib build error

9,491件の閲覧回数
MuhammadOmarFar
Contributor I

Hey,

I am performing ltib build operation as shown in  the step 4 in section 2.2 in the document that i have attached.

but this error is coming

"ltib can not run because one or more host packages needed to run it are either missing or out of date or not in ltib's standard path" .

 i am a newbie :( ..can any one help me ?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

9,325件の閲覧回数
RandyKrakora
NXP Employee
NXP Employee

Here's some info here:

http://www.imxdev.org/wiki/index.php?title=ALL_Boards_ltib_config_ubuntu

Make a mental note of this step though -> "Ubuntu distro uses dash instead of bash as shell, then change it to bash:", it probably won't hurt you, but there are some differences in scripting across the two shells.

But either way, I followed the instructions exactly, then ltib worked fine.

-Randy

0 件の賞賛
返信

9,325件の閲覧回数
KrishnaPavan
Contributor II

look in the error log!

0 件の賞賛
返信