lpddr2 DCD table configuration for uboot_v2014.04 for imx6solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpddr2 DCD table configuration for uboot_v2014.04 for imx6solo

Jump to solution
1,649 Views
gbiradar
Contributor IV

Hi Guys,

             i need lpddr2 register script generator for imx_v2014.04_3.14.28_1.0.0_ga for imx6solo. i have used Mx6DQSDL LPDDR2 Script Aid V0.04.xlsx but it is of no help.

thanks in advance for your help

Ganesh

Labels (2)
0 Kudos
Reply
1 Solution
1,406 Views
gbiradar
Contributor IV

sudo dd if=u-boot.imx of=/dev/sdX bs=512 seek=2

View solution in original post

0 Kudos
Reply
2 Replies
1,406 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh

I am not aware of "script generators" tool, as for Solo lpddr2 settings one can look at

i.MX 6Solo LPDDR2 Registry Settings

imx6 bootloader - kernel bad CRC

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,407 Views
gbiradar
Contributor IV

sudo dd if=u-boot.imx of=/dev/sdX bs=512 seek=2

0 Kudos
Reply