Hello,
I would like to ask question how to load image from SD-card with U-boot running.
My setup is:
- U-boot loaded to i.MX6sl through serial download mode (because I compile under Linux, I have been using imx_usb to put U-boot on board)
- I have serial console working and steps I set:
Hit any key to stop autoboot: 0
U-Boot > setenv loadaddr 0x80800000
U-Boot > setenv bootargs_base 'setenv bootargs console=ttymxc0,115200'
U-Boot > setenv kernel 'uImage'
U-Boot > setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw'
U-Boot > setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc dev 2;mmc read ${loadaddr} 0x800 0x1800;bootm
U-Boot > setenv bootcmd 'run bootcmd_mmc'
U-Boot > saveenv
Saving Environment to MMC...
Writing to MMC(2)... done
U-Boot > run bootcmd
mmc2 is current device
MMC read: dev # 2, block # 2048, count 6144 ... 6144 blocks read: OK
Wrong Image Format for bootm command
ERROR: can't get kernel image!
I am using SD3 so card is seen on 2nd port.
I think that problem is with proper path settings to uImage (I wish to see line 'Uncompressing Linux....')
Card I am using have 2 partitions 1st fat bootable, 2nd Linux partition:
:~/$ cat /proc/partitions
major minor #blocks name
| 8 | 49 | 8192 sdd1 | 
| 8 | 50 | 544768 sdd2 | 
How should I change my setting to be able to load from /sdd2/boot/uImage ?
uImage info:
Image Name: Linux-3.0.35-02887-g731b440-dirt
Created: Mon Nov 23 14:49:09 2015
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3567572 Bytes = 3483.96 kB = 3.40 MB
Load Address: 10008000
Entry Point: 10008000
Image arch/arm/boot/uImage is ready
HI Pawel
/dev/mmcblk0 corresponds to MMC/SD Slot 1 as
described on p.25 attached i.MX6SL EVK Linux Guide.
Also it may be useful to look at Release Notes
Table 7. Kernel Boot Parameters
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Realy apprechiate how much You are helping. Thank You a lot. It takes me some time for me to figure it out since I was trying to download kernel through serial (possible) and to build descent one for my usage. So now I am step closer to success. So my situation is:
I have SD card with two partitions:
1st fat
2nd ext3
I can 'boot' uImage from both (fatload mmc 0:1 0x80800000 uImage) (ext2load mmc 0:2 0x80800000 /boot/uImage) but for this content lets assume that I have been using 2nd partition ext3.
I can list it:
MX6Sl EVK U-Boot > mmc dev 0
mmc0 is current device
MX6Sl EVK U-Boot > ext2ls mmc 0:2
<DIR> 4096 .
<DIR> 4096 ..
<DIR> 16384 lost+found
<DIR> 4096 mnt
<DIR> 4096 var
<DIR> 4096 etc
<DIR> 4096 lib
<DIR> 4096 usr
<DIR> 4096 opt
<DIR> 4096 home
<DIR> 4096 boot
<DIR> 4096 sys
<DIR> 4096 bin
<DIR> 4096 proc
<DIR> 4096 run
<DIR> 4096 dev
<DIR> 4096 unit_tests
<DIR> 4096 sbin
<DIR> 4096 tmp
<DIR> 4096 media
So I can say that this is not hardware problem.
Ok. So I am loading it and run:
MX6Sl EVK U-Boot > ext2load mmc 0:2 0x80800000 /boot/uImage
Loading file "/boot/uImage" from mmc device 0:2 (xxa2)
3330308 bytes read
MX6Sl EVK U-Boot > bootm 0x80800000
## Booting kernel from Legacy Image at 80800000 ...
Image Name: Linux-3.0.35-02887-g731b440-dirt
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3330244 Bytes = 3.2 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ...
Everything goes quite nice untill it try to mount filesystem (I try mtdblock2 since I expect there will be filesystem)
VFS: Cannot open root device "mtdblock2" or unknown-block(0,0)
Please append a correct "root=" boot option; here are the available partitions:
1f00 64 mtdblock0
(driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
And when I try to mount only one visible mtdblock0 (size 64 -> definitely sth is wrong here)
jffs2: Too few erase blocks (2)
List of all partitions:
1f00 64 mtdblock0 (driver?)
No filesystem could mount root, tried: jffs2
Of course jffs2/ext3 no difference.
My idea was that there were missing drivers for ext3, but they are build in kernel (*file.png).
I attach whole log (close.txt) if some more info is needed.
Any ideas? Hint? Any help will be great ![]()
Ok I am closer ![]()
"host SD card with different parameters than your own U-Boot" <-- there were key.
I change card MUX setting on configuration files.
(had 8bit support while using only 4 to communicate with SD).
For other have same problem look at (board-mx6...c with SD cards and headers board-mx6...common.h and iomux-mx6...h)
Now kernel command line look:
Kernel command line: noinitrd console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw rootfstype=ext3 ip=off
now partitions are visible.
VFS: Cannot open root device "mmcblk0p2" or unknown-block(179,2)
Please append a correct "root=" boot option; here are the available partitions:
mmc1: mmc_rescan_try_freq: trying to init card at 100000 Hz
1f00 64 mtdblock0 (driver?)
b300 3931136 mmcblk0 driver: mmcblk
b301 204800 mmcblk0p1 00000000-0000-0000-0000-000000000000
b302 3725312 mmcblk0p2 00000000-0000-0000-0000-000000000000
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)
so close but why it is not booting since it looks ok?
HI Pawel
what board/Linux distribution you are using,
Is it freescale from i.MX6SL EVK product page ?
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6SLEVK&fpsp=1&tab=Design_Tools_Tab
Also you are using kernel command line:
noinitrd console=ttymxc0,115200 root=/dev/mtdblock0 rw rootfstype=jffs2 ip=off
Had you read suggested attached documents, it never show such command line.
Best regards
igor
Board based on i.MX6SL EVK (thats why I am using sources from this board).
Linux:
git://github.com/embest-tech/linux-imx.git -b embest_imx_3.0.35_4.0.0
Which has imx6s_defconfig and have support to imx6sl processors (support.png)
Yes I think I read almost every one more than once.
usually they advice sth like:
root=/dev/mmcblkXpY
while kernel doesn't see any partition available except mtdblock0. If I set boot_comand to mount root from /dev/mmcblkXpY error is same as 1st log:
VFS: Cannot open root device "mtdblock2" or unknown-block(0,0)
later jffs or ext.. doesn't metter since kernel can't find device.
for embest distribution please post this to
meta-fsl-arm mailing list, so that someone familiar with that board could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
igor