load images in imx8mm-evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

load images in imx8mm-evk

Jump to solution
5,323 Views
inigovicentewal
Contributor III

Hi, 

I am using iMX8M Mini EVK to flash an image.
I don't know what exit I should give but I think it's wrong.
I am following the instructions below:

Get Started with the i.MX 8M Mini EVK | NXP 

How to use UUU on Windows · NXPmicro/mfgtools Wiki · GitHub 

On Windows Host side the console shows:

C:\Users\ivicente\Desktop\imx\L4.14.98_2.0.0_ga_images_MX8MMEVK>uuu.exe -v -b uuu.auto
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.102-0-gb078bd0

Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02

Run built-in script:
uuu_version 1.2.39

# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -offset 0x57c00
SDPU: jump
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -skipspl
SDPV: jump
# }

FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}
FB: flash -raw2sparse all fsl-image-validation-imx-imx8mmevk.sdcard
FB: flash bootloader imx-boot-imx8mmevk-sd.bin-flash_evk
FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: done

Wait for Known USB Device Appear...
New USB Device Attached at 2:1
2:1>Start Cmd:SDP: boot -f imx-boot-imx8mmevk-sd.bin-flash_evk
6400%2:1>Okay (0.629s)
New USB Device Attached at 2:1
2:1>Start Cmd:SDPV: delay 1000
2:1>Okay (1.003s)
2:1>Start Cmd:SDPV: write -f imx-boot-imx8mmevk-sd.bin-flash_evk -skipspl
100%2:1>Okay (1.41s)
2:1>Start Cmd:SDPV: jump
6400%2:1>Okay (0.311s)

On mx8mm-evk side the debug console shows:

U-Boot SPL 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Apr 11 2019 - 11:14:18 +0000)
power_bd71837_init
DDRINFO: start lpddr4 ddr init
DRAM PHY training for 3000MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 400MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 100MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DRAM PHY training for 3000MTS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training PASS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from USB SDP
SDP: initialize...
SDP: handle requests...
Downloading file of size 1231584 to 0x40400000... done
Jumping to header at 0x40400000
Header Tag is not an IMX image
Found header at 0x4042b400


U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Apr 11 2019 - 11:14:18 +0000)

CPU: Freescale i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 34C
Reset cause: POR
Model: FSL i.MX8MM EVK board
DRAM: 2 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
Power supply on USB2
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... Card did not respond to voltage select!
*** Warning - No block device, using default environment

Failed (-5)
No panel detected: default to MIPI2HDMI
adv7535_init: Can't find device id=0x3d, on bus 1
Display: MIPI2HDMI (1920x1080)
Video: 1920x1080x24
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF 1cb68fa
- U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df

Card did not respond to voltage select!
Detect USB boot. Will enter fastboot mode!
Net:
Warning: ethernet@30be0000 using MAC address from ROM
eth0: ethernet@30be0000
Fastboot: Normal
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
Hit any key to stop autoboot: 0

## Checking Image at 43800000 ...
Unknown image format!
Run fastboot ...
g_dnl_register: failed!, error: -19
u-boot=>

I think this is not the normal boot, does anyone know how to fix this?

I am using usb adapter type c male to type a female instead of type a male to micro b male to debug. Can i cause the error?

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
4,819 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, 4.14.98 includes op-tee, for more detailed information, pls refer to the release note of 4.14.98

View solution in original post

0 Kudos
Reply
7 Replies
4,820 Views
joanxie
NXP TechSupport
NXP TechSupport

I used “uuu.exe uuu.auto" successfully, after program, did you boot up the board successfully? could you send the log file to me when the board boot up if the board failed?

0 Kudos
Reply
4,819 Views
inigovicentewal
Contributor III

Hi joanxie

I already solved my problem, thanks

Another question, Do you know if the OP-TEE project is integrated in L4.14.98_2.0.0_ga_images_MX8MMEVK?

It's right?

TFA is also activated? If not, how can I do it?

0 Kudos
Reply
1,951 Views
AlekseyM
Contributor III

could you add solving for "Header Tag is not an IMX image" I have the same issues with u-boot on the same address

0 Kudos
Reply
4,820 Views
nayanan996
Contributor I

Hi Iñigo Vicente,

I too am facing the same problem. Can you please elaborate on how you solved the error. I too am getting in the end.

g_dnl_register: failed!, error: -19

U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Apr 11 2019 - 11:14:18 +0000)

CPU: Freescale i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 34C
Reset cause: POR
Model: FSL i.MX8MM EVK board
DRAM: 2 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
Power supply on USB2
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... Card did not respond to voltage select!
*** Warning - No block device, using default environment

Failed (-5)
No panel detected: default to MIPI2HDMI
adv7535_init: Can't find device id=0x3d, on bus 1
Display: MIPI2HDMI (1920x1080)
Video: 1920x1080x24
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF 1cb68fa
- U-Boot 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df

Card did not respond to voltage select!
Detect USB boot. Will enter fastboot mode!
Net:
Warning: ethernet@30be0000 using MAC address from ROM
eth0: ethernet@30be0000
Fastboot: Normal
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
Hit any key to stop autoboot: 0

## Checking Image at 43800000 ...
Unknown image format!
Run fastboot ...
g_dnl_register: failed!, error: -19
u-boot=>

0 Kudos
Reply
4,820 Views
inigovicentewal
Contributor III

Hi,

In my case it was because the Type C connector Port 1 (J301 Download) that came with the kit was not connected. In short, from my experience, you cannot use another type C connector other than the kit.
You can see this other thread with the same problem:unable to load images onto imx8mm-evk

Best regards,

Iñigo

4,820 Views
mahesh_rd
Contributor I

But in my case, the download of demo images were fine when I tired with the same wires. It only happens for my custom baked images.

0 Kudos
Reply
4,820 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, 4.14.98 includes op-tee, for more detailed information, pls refer to the release note of 4.14.98

0 Kudos
Reply