Hi chavira,
i was followed your instructions still i am facing same issue. Need your support
oly@BSP:~/Documents/BSP-Yocto/build-xwayland$ bitbake -c fetch virtual/kernel
Loading cache: 100% |##########################################################################################################| Time: 0:00:05
Loaded 5717 entries from dependency cache.
Parsing recipes: 100% |########################################################################################################| Time: 0:00:01
Parsing of 3642 .bb files complete (3640 cached, 2 parsed). 5718 targets, 388 skipped, 17 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "2.8.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8qxpc0mek"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "6.6-scarthgap"
TUNE_FEATURES = "aarch64 armv8a crc crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:f43f393ef0246b7bee6eed8bcf8271cf2b8cdf40"
meta-oe
meta-multimedia
meta-python = "HEAD:80e01188fa822d87d301ee71973c462d7a865493"
meta-freescale = "HEAD:0f8091c63dd8805610c09b08409bc58492a3b16f"
meta-freescale-3rdparty = "HEAD:6c063450d464eb2f380443c7d9af1b94ce9b9d75"
meta-freescale-distro = "HEAD:b9d6a5d9931922558046d230c1f5f4ef6ee72345"
meta-imx-bsp
meta-imx-sdk
meta-imx-ml
meta-imx-v2x = "HEAD:6bbf35e73f1b537b19be830462af87a3bd68e1ab"
meta-nxp-demo-experience = "HEAD:8fd7154c05b716e9635279047f65785399432d88"
meta-nxp-matter-baseline
meta-nxp-openthread = "HEAD:783becb4b5716d989f50db95b7133d38eae5b47b"
meta-arm
meta-arm-toolchain = "HEAD:1b85bbb4cab9658da3cd926c62038b8559c5c64e"
meta-clang = "HEAD:fe561f41aef0cff9e6f96730ab59f28dca2eb682"
meta-gnome
meta-networking
meta-filesystems = "HEAD:80e01188fa822d87d301ee71973c462d7a865493"
meta-qt6 = "HEAD:dc13e1bfda4a4757a08c2d6673bc4bac012c4a80"
meta-parsec
meta-tpm = "HEAD:11ea91192d43d7c2b0b95a93aa63ca7e73e38034"
meta-virtualization = "HEAD:6a80f140e387621f62964209a2e07d3bcfb125ce"
Sstate summary: Wanted 0 Local 0 Mirrors 0 Missed 0 Current 1 (0% match, 100% complete)############################# | ETA: 0:00:00
Initialising tasks: 100% |#####################################################################################################| Time: 0:00:00
NOTE: Executing Tasks
WARNING: linux-imx-6.6.36+git-r0 do_fetch: Failed to fetch URL git://github.com/nxp-imx/linux-imx.git;protocol=https;branch=lf-6.6.y, attempting MIRRORS if available
ERROR: linux-imx-6.6.36+git-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/oly/Documents/BSP-Yocto/build-xwayland/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/oly/Documents/BSP-Yocto/sources/poky/scripts:/home/oly/Documents/BSP-Yocto/build-xwayland/tmp/work/imx8qxpc0mek-poky-linux/linux-imx/6.6.36+git/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/oly/Documents/BSP-Yocto/build-xwayland/tmp/work/imx8qxpc0mek-poky-linux/linux-imx/6.6.36+git/recipe-sysroot/usr/bin/crossscripts:/home/oly/Documents/BSP-Yocto/build-xwayland/tmp/work/imx8qxpc0mek-poky-linux/linux-imx/6.6.36+git/recipe-sysroot-native/usr/sbin:/home/oly/Documents/BSP-Yocto/build-xwayland/tmp/work/imx8qxpc0mek-poky-linux/linux-imx/6.6.36+git/recipe-sysroot-native/usr/bin:/home/oly/Documents/BSP-Yocto/build-xwayland/tmp/work/imx8qxpc0mek-poky-linux/linux-imx/6.6.36+git/recipe-sysroot-native/sbin:/home/oly/Documents/BSP-Yocto/build-xwayland/tmp/work/imx8qxpc0mek-poky-linux/linux-imx/6.6.36+git/recipe-sysroot-native/bin:/home/oly/Documents/BSP-Yocto/sources/poky/bitbake/bin:/home/oly/Documents/BSP-Yocto/build-xwayland/tmp/hosttools"; export HOME="/home/oly"; LANG=C git -c gc.autoDetach=false -c core.pager=cat -c safe.bareRepository=all clone --bare --mirror
https://github.com/nxp-imx/linux-imx.git /home/oly/Documents/BSP-Yocto/downloads//git2/github.com.nxp-imx.linux-imx.git --progress failed with exit code 128, see logfile for output
ERROR: linux-imx-6.6.36+git-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/nxp-imx/linux-imx.git;protocol=https;branch=lf-6.6.y')
ERROR: Logfile of failure stored in: /home/oly/Documents/BSP-Yocto/build-xwayland/tmp/work/imx8qxpc0mek-poky-linux/linux-imx/6.6.36+git/temp/log.do_fetch.43985
ERROR: Task (/home/oly/Documents/BSP-Yocto/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2 tasks of which 1 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/oly/Documents/BSP-Yocto/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_fetch
Summary: There was 1 WARNING message.
Summary: There were 2 ERROR messages, returning a non-zero exit code.