linux-imx-5.15.52+gitAUTOINC+36363d8623-r0 do_fetch: Failed to fetch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

linux-imx-5.15.52+gitAUTOINC+36363d8623-r0 do_fetch: Failed to fetch

1,553 次查看
Jimmychea
Contributor III

I got this de_fetch error when building yocto on imx8m plus.

ERROR: linux-imx-5.15.52+gitAUTOINC+36363d8623-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AGENT_PID="1777"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/kcchea/Desktop/imx-yocto-bsp/temp_build/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/kcchea/Desktop/imx-yocto-bsp/sources/poky/scripts:/home/kcchea/Desktop/imx-yocto-bsp/temp_build/tmp/work/imx8mp_lpddr4_evk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/kcchea/Desktop/imx-yocto-bsp/temp_build/tmp/work/imx8mp_lpddr4_evk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/recipe-sysroot/usr/bin/crossscripts:/home/kcchea/Desktop/imx-yocto-bsp/temp_build/tmp/work/imx8mp_lpddr4_evk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/recipe-sysroot-native/usr/sbin:/home/kcchea/Desktop/imx-yocto-bsp/temp_build/tmp/work/imx8mp_lpddr4_evk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/recipe-sysroot-native/usr/bin:/home/kcchea/Desktop/imx-yocto-bsp/temp_build/tmp/work/imx8mp_lpddr4_evk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/recipe-sysroot-native/sbin:/home/kcchea/Desktop/imx-yocto-bsp/temp_build/tmp/work/imx8mp_lpddr4_evk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/recipe-sysroot-native/bin:/home/kcchea/Desktop/imx-yocto-bsp/sources/poky/bitbake/bin:/home/kcchea/Desktop/imx-yocto-bsp/temp_build/tmp/hosttools"; export HOME="/home/kcchea"; LANG=C git -c core.fsyncobjectfiles=0 -c gc.autoDetach=false -c core.pager=cat clone --bare --mirror https://github.com/nxp-imx/linux-imx.git /home/kcchea/Desktop/imx-yocto-bsp/downloads//git2/github.com.nxp-imx.linux-imx.git --progress failed with exit code 128, no output
ERROR: linux-imx-5.15.52+gitAUTOINC+36363d8623-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/nxp-imx/linux-imx.git;protocol=https;branch=lf-5.15.y')
ERROR: Logfile of failure stored in: /home/kcchea/Desktop/imx-yocto-bsp/temp_build/tmp/work/imx8mp_lpddr4_evk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/temp/log.do_fetch.730435
ERROR: Task (/home/kcchea/Desktop/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-kernel/linux/linux-imx_5.15.bb:do_fetch) failed with exit code '1'

标记 (2)
0 项奖励
回复
1 回复

1,430 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

It maybe caused by the network problem, you can follow our i.MX Yocto Project User’s Guide​ document for download source code and compile BSP Documentation

0 项奖励
回复