hi,
i just got involved in a project on a board modified from imx6dlsabresd recently.
i have built the core-image-minimal and meta-toolchain by yocto / bitbake with source from fsl-community-bsp 2.1.2 (kernel 4.1).
when further worked on an application based on imx-test,
i found that the fb.h in build/tmp/sysroots/imx6dlsabresd/usr/include/linux differs from the one in kernel source.
can someone explain to me what the two versions are?
(i traced and found that when compiling imx-test with bitbake the real header file included is the "original" one from the kernel source : build/tmp/work-shared/imx6dlsabresd/kernel-source/include)
In addition, if we want to develop applications with but outside yocto, which "include"s and "lib"s in the build/tmp are the ones we should include / linked against?
paul wang.
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Paul
differencies may be explained by community BSP and official release BSPs as explained on
https://community.freescale.com/message/402940#402940
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------