linux/arch/arm (mxs mxc imx) Confused

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

linux/arch/arm (mxs mxc imx) Confused

ソリューションへジャンプ
3,449件の閲覧回数
preb
Contributor I

I am going to do some developent for imx25 from freescale.

When looking into the linux/arc/arm folder, I am confused with the structure.

I see mxs, mxc and imx "platform" files. I get the felling that, some is old, and some is the new way.

Can someone explain the history and plans for the "platform structure" for imx arm?


ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
1,681件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

It is because the BSP support different i.MX products, some drivers are not used for i.MX25.

Mostly, the filename will starting with mx25_xxx means this is specially for i.MX25.

Do you have i.MX25PDK board?

You can order the i.MX25PDK board for your application development.

Here is the i.MX25PDK web page:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK

You can download all the useful documents (App Notes), BSP source code and tools from this web page.

Please download the IMX25_0912_SDK_LINUXDOCS_BUNDLE.

There is a i.MX25 BSP reference manual which talk about the i.MX25PDK drivers in the BSP in details. such as which is the driver .c and .h file, where is the file location in the source code.. etc.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,682件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

It is because the BSP support different i.MX products, some drivers are not used for i.MX25.

Mostly, the filename will starting with mx25_xxx means this is specially for i.MX25.

Do you have i.MX25PDK board?

You can order the i.MX25PDK board for your application development.

Here is the i.MX25PDK web page:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX25PDK

You can download all the useful documents (App Notes), BSP source code and tools from this web page.

Please download the IMX25_0912_SDK_LINUXDOCS_BUNDLE.

There is a i.MX25 BSP reference manual which talk about the i.MX25PDK drivers in the BSP in details. such as which is the driver .c and .h file, where is the file location in the source code.. etc.

0 件の賞賛
返信
1,681件の閲覧回数
csoapy
Contributor III

It's still not clear what's 's', 'c' in mxs/mxc stands for.

And other file names which start with imx... and mx..., so what's the difference of imx & mx?

0 件の賞賛
返信
1,681件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

There is no standard for the names.

There is Linux Reference manual contain the details of the drivers. (i.MX_Reference_Manual.pdf)

e.g. L4.14.78 BSP documentation

Linux L4.14.78_1.0.0 Documentation

0 件の賞賛
返信