linux_5.10.9_1.0.0/sources/meta-qt5/recipes-qt/qt5/qtwayland_git.bb:do_configure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

linux_5.10.9_1.0.0/sources/meta-qt5/recipes-qt/qt5/qtwayland_git.bb:do_configure

ソリューションへジャンプ
2,245件の閲覧回数
ttttttx
Contributor III

 

Re: fail to sync yocto (Linux 5.10.9_1.0.0) On Chi... - NXP Community

When I built imx-image-full, I found that qtwangland always failed to compile.

1.png

2.png

3.png

Test config.qtwayland_client.tests.dmabuf-server-buffer tries to use undeclared library 'drm'

lib drm ?

 

4.png

 

I had cleanall-ed them and rebuild , but no effect

 

How to solve this problem ?

 

 

0 件の賞賛
返信
1 解決策
2,216件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport
1 返信
2,217件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi raotianxiang

 

Try this patch :https://codereview.qt-project.org/c/qt/qtwayland/+/296213